Principles of Reliability Engineering in Power Electronics
Reliability engineering in power electronics is a crucial field concerned with maintaining the long-term operational stability and dependability of electronic systems under a variety of conditions. As power electronics are employed in more demanding applications, ranging from industrial machines to aerospace systems, the requirement to design for reliability has never been more significant. This section delves into the fundamental principles of reliability engineering in power electronics, including key factors that influence reliability, methods for predicting and improving reliability, and the significance of incorporating reliability considerations throughout the design and development process.
Reliability in Power Electronics
The ability of a system or component to carry out its intended function under specified conditions for a defined period without failing is referred to as reliability in the context of power electronics. Even in the face of environmental stresses including temperature swings, humidity, electrical noise, and mechanical vibration, a highly reliable power electronic system continuously performs within its performance parameters.
Key Reliability Metrics:
Mean Time Between Failures (MTBF): MTBF is a statistical measure of a system or component's average time between failures. It is an important indicator of reliability, especially in systems that require continuous operation.
$$ \text{MTBF} = \frac{\text{Total operational time}}{\text{Number of failures}} $$Failure Rate: The frequency of system or component failures over time is known as the failure rate. It is frequently represented as failures per unit of time (e.g., failures per hour) and is inversely proportional to MTBF.
$$ \text{Failure rate} = \frac{1}{\text{MTBF}} $$Availability: The proportion of time that a system is operational and able to perform its intended purpose is referred to as availability. It is affected by the system's reliability as well as how well maintenance and repair procedures.
$$ \text{Availability} = \frac{\text{Uptime}}{\text{Uptime} + \text{Downtime}} $$Factors Influencing Reliability in Power Electronics
Component Quality and Selection: The quality and selection of a power electronic system's components have a significant impact on its reliability. High-quality components made to strict specifications are less likely to have flaws or fail prematurely. When choosing components, designers ought to consider factors including:
- Thermal Ratings: Components having greater thermal ratings can survive the heat generated in power conversion circuits, minimizing the chance of thermal failures.
- Electrical Stress Tolerance: Components should be chosen according to their ability to withstand electrical stresses such as overvoltages, high currents, and switching transients. Reliability can be improved by derating components or utilizing them below their maximum rated values.
- Material Properties: Under operating conditions, the materials used in capacitors, semiconductors, and other components must be reliable. For instance, applications needing long-term reliability favor ceramic capacitors with strong dielectric stability.
Thermal Management: For power electronics to remain reliable, effective thermal control is essential. Overheating can hasten component wear and deterioration, resulting in early failures. In order to guarantee that components operate within safe temperature ranges, reliable systems are built using strong thermal management techniques, such as adequate heat sinks, cooling systems, and thermal interface materials (TIMs).
Environmental Considerations: Power electronic systems frequently operate in harsh conditions where dust, vibration, and humidity can affect reliability. Designing resilient designs for the environment entails:
- Sealing and Encapsulation: Assemblies and components can be encased or sealed to keep out dust, moisture, and corrosive environments.
- Vibration Resistance: To avoid fatigue and failure of solder joints, connectors, and other mechanical interfaces, systems exposed to mechanical vibration must be designed with robust mounting and shock-absorbing materials.
Electromagnetic Compatibility (EMC): Ensuring that power electronic systems are electromagnetically compatible with their environment is vital for reliability. Electromagnetic interference (EMI) and other EMC issues can interfere with sensitive components' ability to function, resulting in failure or malfunction. In order to reduce electromagnetic interference (EMI) and preserve steady operation, reliable designs incorporate appropriate shielding, filtering, and grounding techniques.
Reliability Prediction and Modeling
Reliability Prediction Methods: A power electronic system's reliability can be predicted by estimating failure rates and MTBF using statistical models and historical data. Common methods include:
- Parts Count Method: This method estimates a system's reliability by calculating the failure rates of its individual components and adjusting for environmental and operating conditions. It offers a rapid system reliability estimate that is useful in the early phases of design.
- Stress-Strength Analysis: This method compares the strength of the component (e.g., rated voltage, maximum operating temperature) with the applied stresses (e.g., voltage, current, temperature) in order to assess the reliability of the component. Because it is not practical to do this analysis for every component, it is only done for the most crucial ones. A system is more reliable when its components have a better strength-to-stress ratio since they are less likely to fail.
- Reliability Block Diagrams (RBDs): RBDs visually depict the configuration of system components and how their reliability contributes to overall system reliability. Based on component reliabilities, series and parallel configurations are examined to forecast the probability of system failure.
Figure 16: Sample stress-strength analysis
Figure 17: Reliability block diagram (ʎ is failure rate)
Failure Modes and Effects Analysis (FMEA): FMEA is a methodical approach for identifying potential failure modes in a system, evaluating their impact, and setting priorities for actions to minimize these risks. FMEA assists engineers in identifying crucial areas that may jeopardize reliability and development strategies to address them by examining every component and subsystem.
Accelerated Life Testing (ALT): ALT involves subjecting components or systems to heightened stress levels, such as higher temperatures or voltages, to accelerate the aging process and detect possible failure mechanisms. The data gathered via ALT can be utilized to validate reliability models and forecast the system's reliability under normal operating conditions.
Design for Reliability
Redundancy and Fault Tolerance: Redundancy is frequently used in high-reliability systems to guarantee continuous operation even in the event of a component failure. Parallel components, backup circuits, or failover mechanisms that automatically switch to a backup system in the event of a failure are examples of redundant systems. Design techniques such as error detection and correction, which enable the system to function even in the face of malfunctions, are another way to achieve fault tolerance.
Design for Maintainability: Reliability engineering also analyzes how easy it is to maintain and repair the system. Modular components that can be quickly replaced, clear diagnostics to indicate failed components, and accessible layouts to aid repairs are all aspects of maintainability-designed systems. An easy-to-maintain design will have a longer operational life and less downtime, increasing overall reliability.
Continuous Improvement: Reliability engineering is a continual process that persists after the initial design phase. Continuous improvement entails gathering and analyzing field data on failures, updating reliability models, and adjusting designs based on real-world performance. Feedback loops between design, testing, and field operations assist guarantee that reliability objectives are met and maintained throughout the product's lifecycle.
Strategies for Enhancing System Efficiency
System efficiency is an important feature of power electronics design, as it has a direct impact on electronic system performance, operational costs, and environmental footprint. Improving efficiency entails reducing energy losses during power conversion and ensuring that the system performs effectively under various conditions. The main tactics for improving power electronics system efficiency are described in this section, with an emphasis on circuit design, component selection, control methods, and thermal management.
Component Selection and Optimization
High-Efficiency Semiconductor Devices: The overall efficiency of a power conversion system is largely determined by the selection of semiconductor devices, including diodes, MOSFETs, and IGBTs. Here are some strategies for optimizing component selection:
- Low On-Resistance Devices: Low on-resistance MOSFETs minimize conduction losses, particularly in applications where the device conducts current for prolonged periods of time. Higher efficiency is directly related with lower conduction losses.
- Fast Switching Devices: Devices with high switching speeds, including Gallium Nitride (GaN) and Silicon Carbide (SiC) transistors, provide lower switching losses, which are essential for increasing high-frequency power converter efficiency. These devices are perfect for modern high-efficiency designs because they allow for faster switching transitions with reduced energy dissipation.
- Soft Recovery Diodes: Reverse recovery losses, which happen when the diode transitions from conducting to blocking mode, can be minimized by using diodes with smooth recovery characteristics. Soft recovery diodes contribute to increased system efficiency by reducing power losses and associated switching noise.
Passive Component Optimization: The efficiency of the system is also significantly affected by passive components such as transformers, capacitors, and inductors. The following are some strategies for improving efficiency through passive component optimization:
- Low Loss Magnetic Materials: Choosing inductors and transformers with cores composed of low-loss magnetic materials decreases core losses, especially at high switching frequencies. For instance, ferrite cores are frequently utilized due to their low eddy current losses and hysteresis.
- High-Frequency Capacitors: Capacitors with high ripple current ratings and low equivalent series resistance (ESR) are crucial for reducing power dissipation and increasing efficiency in high-frequency applications. These capacitors continue to function steadily when switching at high frequencies.
- Minimizing Parasitic Elements: Unwanted resonances and energy losses can be introduced by parasitic capacitance and inductance in the circuit. Careful layout design, appropriate component selection, and the incorporation of shielding techniques can help to reduce parasitics and increase system efficiency.
Circuit Design Techniques
Topology Selection: The efficiency of the system is significantly impacted by the power converter topology selection. Because they can reduce losses, certain topologies are by inherently more efficient:
- Resonant Converters: Resonant converters, such as LLC resonant converters, work by switching at the circuit's natural resonant frequency, reducing switching losses and enabling soft switching. Because of their excellent efficiency, these topologies are frequently employed in applications that need low electromagnetic interference (EMI) and high-power density.
- Synchronous Rectification: Synchronous rectification substitutes traditional diodes with actively regulated MOSFETs, which greatly reduces conduction losses during the rectification stage. This approach is especially useful in low-output voltage, high-current applications, such as power supplies for consumer electronics.
- Interleaved and Multi-Phase Designs: By distributing the load current throughout parallel phases, interleaving multiple converter stages helps smooth the input and output current waveforms and lessen the strain on individual components. This method increases overall efficiency by lowering conduction losses and enhancing thermal management.
Figure 18: (a) Diode rectifier (b) Synchronous rectifier
Minimizing Switching and Conduction Losses: Efficient circuit design requires minimizing switching and conduction losses. Significant strategies consists:
- Optimizing Dead Time: Dead time in power converters is the period of time when the low-side and high-side switches are deactivated to avoid short circuiting. On the other hand, too much dead time may result in higher conduction losses. Optimizing dead time to the shortest possible duration reduces losses and increases efficiency.
- Gate Drive Optimization: Achieving efficient switching transitions requires proper gate drive design. Fast, regulated gate drive signals reduce switching losses by ensuring that transistors turn on and off fast and without excessive overshoot or ringing (oscillatory behavior at MOSFET/IGBT gate terminals during switching events), which can lead to energy dissipation.
- Snubber Circuits: Snubber circuits are designed to protect power switches against voltage spikes induced by parasitic inductances. By lessening the energy lost in these spikes and avoiding needless power dissipation, well-designed snubbers can further enhance efficiency.
Advanced Control Techniques
Dynamic Power Management: Dynamic power management involves adjusting the power converter's operating conditions to match requirements for load. This approach lowers power consumption during periods of low demand, increasing efficiency:
- Pulse-Width Modulation (PWM) Adjustments: The converter can sustain high efficiency under a variety of operating conditions by dynamically modifying the PWM signal's duty cycle in response to the load conditions. For instance, switching losses can be reduced by lowering the duty cycle when there is less load.
- Variable Frequency Operation: To maximize efficiency, the operating frequency of some converters can be adjusted in response to load conditions. Higher frequencies can be used to sustain performance under heavy loads, whereas lower frequencies minimize switching losses during light-load operation.
Digital Control and Adaptive Techniques: Digital control enables more precise and adaptive regulation of power converters, resulting in increased efficiency:
- Adaptive Dead Time Control: Digital controllers can dynamically change dead time in response to changing load conditions, reducing dead time losses and limiting cross-conduction.
- Adaptive Voltage Scaling: In microprocessors, adaptive voltage scaling (AVS) reduces power consumption and improves efficiency by adjusting the supply voltage to the lowest amount required for a given performance level.
- Predictive Control: Predictive control algorithms anticipate changes in load conditions and alter converter operation proactively, reducing transient losses while maintaining high efficiency during dynamic operation.
Thermal Management for Efficiency
Thermal Design and Efficiency: Overall system efficiency is directly related to efficient thermal management. Thermal management systems prevent components from operating at high temperatures, which can increase losses and decrease efficiency, by efficiently dissipating heat:
- Optimized Heat Sink Design: Heat sinks with appropriate fin designs, materials, and surface treatments can improve heat dissipation, allowing components to operate within their optimal temperature range while being highly efficient.
- Active Cooling Solutions: Active cooling solutions, such as fans, blowers, or liquid cooling systems, are used in high-power applications to enhance heat dissipation and enable the system to operate at higher power levels without compromising efficiency.
- Thermal Interface Materials (TIMs): Thermal resistance between components and heat sinks must be reduced with high-quality TIMs to ensure efficient heat transfer and avoid thermal bottlenecks that could reduce efficiency.
Balancing Cost, Efficiency, and Reliability
Finding the ideal balance between cost, efficiency, and reliability in power electronics design is a difficult but crucial challenge. These three factors are frequently interrelated with improvements in one area leading to trade-offs in another. For instance, increasing system efficiency may result in higher costs, yet concentrating only on cost reduction may jeopardize reliability. The principles and strategies for striking a balance amongst these variables are explored in this section, guaranteeing that power electronic systems meet performance requirements while continuing to be reliable and economically viable in the long run.
The Interrelationship Between Cost, Efficiency, and Reliability
Efficiency vs. Cost: Higher efficiency in power electronics frequently requires the use of advanced materials, more sophisticated components, and complex design techniques, all of which can raise the total cost of the system. Wide-bandgap semiconductors, such as silicon carbide (SiC) or gallium nitride (GaN), for example, have better electrical characteristics and can greatly increase efficiency. However, these materials are more expensive than traditional silicon-based components. Designers must determine if the advantages of enhanced efficiency, such as decreased energy consumption and operating expenses, outweigh the higher initial investment.
Reliability vs. Cost: Another important factor that might raise expenses is reliability. Using more costly components with improved durability, higher thermal ratings, and more stringent quality standards is frequently necessary to provide high reliability. The cost is further increased by using fault-tolerant designs and redundant systems to increase reliability. However, the lower maintenance, repair, and failure-related costs over the system's lifecycle frequently outweigh the higher initial costs in applications where downtime or failure is extremely costly, such as in aerospace, military, or industrial settings.
Efficiency vs. Reliability: Reliability and efficiency can have a complicated relationship. High-efficiency designs often reduce power losses, resulting in reduced operating temperatures and increased reliability. However, pushing the limits of efficiency, such as operating at extremely high frequencies or employing components with limited safety margins, could lead to risks that jeopardize reliability. Ensuring that efficiency increases do not jeopardize system reliability is an important design aspect.
Strategies for Balancing Cost, Efficiency, and Reliability
Cost-Benefit Analysis: A systematic cost-benefit analysis is required to determine the trade-offs between cost, efficiency, and reliability. The analysis should consider both the initial costs (component selection and manufacturing charges) and the long-term costs (energy consumption, maintenance, and possible failure costs). The goal is to create a balanced solution that maximizes total value. For example:
- Life-Cycle Cost Analysis (LCCA): This method evaluates the entire cost of ownership during the system's lifespan, which includes original capital costs, operating expenses, maintenance, and disposal costs. The LCCA helps to determine if investment in improved efficiency or reliability upfront will result in long-term cost savings.
- Return on Investment (ROI) and Payback Period: Calculating the ROI and payback period for various design options can assist identify how quickly the benefits of increased efficiency or reliability outweigh the extra costs.
Figure 19: LCCA analysis components
Component Selection and Design Optimization: It's crucial to select components that provide the best possible balance between price, efficiency, and reliability. The following strategies should be taken into account by designers:
- Component Derating: Operating components below their maximum rated specifications, or derating them, can improve reliability without significantly raising costs. This method lessens component stress, resulting in longer component lifespans and fewer failures.
- Modular Design: Modular design techniques can reduce costs by allowing for component scalability and reuse across different products or systems. This technique also improves reliability by allowing for easy replacement of damaged modules without affecting the entire system.
- Value Engineering: Value engineering entails dissecting every component and subsystem to find opportunities to decrease expenses without sacrificing reliability or efficiency. This might include choosing alternative materials, making circuit designs simpler, or getting rid of features that aren't necessary.
Figure 20: Value engineering
Design for Manufacturability (DFM): DFM is a design approach that emphasizes streamlining the manufacturing process to lower expenses without sacrificing quality. DFM can save production costs and increase reliability by minimizing manufacturing defects through the design of products that are simpler to build, assemble, and test. Important DFM strategies consist of:
- Standardization: Standard components and processes can lower costs by leveraging economies of scale and increasing supply chain efficiency. Standardization also increases reliability by ensuring that components are thoroughly tested and widely available.
- Minimizing Assembly Steps: Reducing the number of assembly steps can reduce labor costs and the chance of errors. For instance, employing automated assembly methods or integrated components might improve reliability and cost efficiency.
Thermal Management and Efficiency: In order to balance reliability and efficiency, effective thermal management is essential. Advanced cooling solutions are necessary to preserve system efficiency and avoid thermal-related breakdowns, even if they can be more expensive. Some strategies are:
- Passive vs. Active Cooling: Although passive cooling solutions, including heat sinks, are usually more reliable and cost-effective, they might not be enough to cool high-power applications. By maintaining lower operating temperatures, active cooling techniques such as fans or liquid cooling can increase efficiency, but they can increase system complexity and cost.
- Optimized PCB Design: Without significantly raising costs, proper PCB layout can increase efficiency and reliability by minimizing hotspots, decreasing thermal resistance, and improving heat dissipation.
Risk Management and Reliability Testing: Implementing strict testing and risk management practices guarantees that efficiency or cost savings will not be gained at the expense of reliability. Among the techniques are:
- Accelerated Life Testing (ALT): To detect potential failure modes and ensure long-term reliability, ALT subjects systems and components to high stress levels. This testing aids in ensuring that unanticipated reliability issues are not introduced by cost or efficiency gains.
- Failure Mode and Effects Analysis (FMEA): Early in the design process, FMEA methodically identifies and addresses potential failure modes, enabling designers to apply affordable solutions that improve reliability without needlessly raising costs.
Custom vs. Off-the-Shelf Solutions: Although it can be more expensive, employing custom components or designs can occasionally offer the optimum balance of reliability and efficiency. On the other hand, off-the-shelf solutions could be more affordable but might not satisfy certain reliability or efficiency requirements. Designers should assess when using standard components is more cost-effective and when a custom solution is justified.
Case Studies and Applications
Consumer Electronics: Cost is frequently the main determinant in consumer electronics, with reliability and efficiency adjusted to satisfy consumer demands. For instance, laptop and smartphone power supplies are made to be extremely efficient in order to prolong battery life, but they are also expensive, necessitating careful component and material selection to strike the right balance.
Automotive Electronics: Due to the safety-critical nature of many systems, including battery management systems (BMS) in electric vehicles, reliability is crucial in automotive applications. The requirement for long-term reliability and high efficiency, especially in challenging conditions, justifies the potential higher cost in this case.
Industrial Power Systems: Reliability and efficiency are frequently given priority above cost in industrial power systems, particularly in applications where downtime is very expensive. Common strategies to guarantee that these systems satisfy strict reliability and efficiency requirements include the use of high-quality components, redundant systems, and robust thermal management.
Techniques for Long-Term Reliability Testing and Assessment
Long-term reliability testing and evaluation are critical components in the development of power electronic systems, especially in applications where failure is not an option, such as aerospace, automotive, and industrial. These strategies ensure that products reach their reliability targets across their intended lifespan by detecting probable failure modes, analyzing the effects of external stressors, and evaluating the design's robustness. This section examines essential long-term reliability testing and assessment methodologies, providing insights into how these methods are used to assure the endurance and reliability of power electronic devices.
Accelerated Life Testing (ALT)
Accelerated Life Testing simulates a product's long-term performance by subjecting it to high-stress conditions such as higher temperatures, increased voltage or current, mechanical vibration, or humidity. The objective is to cause breakdowns more quickly than they would under typical operating circumstances, allowing engineers to spot weaknesses and failure mechanisms.
Types of ALT:
- Temperature-Humidity Bias Testing: In this test, electrical bias is applied while the device is exposed to high humidity and temperatures. It is very helpful in identifying issues related to leakage currents, corrosion, and material deterioration.
- Thermal Cycling: To simulate the thermal expansion and contraction that occurs during normal operation, components are frequently cycled between high and low temperatures. This test aids in the identification of thermal stress-related issues such as solder joint fatigue and material cracking.
- Power Cycling: Power cycling is the process of frequently turning the power on and off to mimic the electrical and thermal stress that components go through during cycles of startup and shutdown. This test is helpful in detecting component wear and thermal fatigue failures.
Figure 21: Solar panel thermal cycling
Analyzing ALT Results: Data from ALT is used to model the product's reliability under normal operating conditions. Common techniques for analysis include:
- Weibull Analysis: The time to failure of systems and components is modeled using this statistical method. It aids in estimating the expected lifespan of the product and forecasting the possibility of failure over time.
- Arrhenius Model: This model is used to calculate the acceleration factor in ALT and the activation energy of failure mechanisms, allowing ALT results to be extrapolated to normal operating conditions. The most prevalent application for this approach is when the stimulus or acceleration variable is thermal.
Highly Accelerated Life Testing (HALT)
Highly Accelerated Life Testing (ALT) is a more aggressive method of testing that pushes products beyond their specified operational limitations in order to discover possible causes of failure. The goal of HALT is to identify the weakest points in the design and production processes, allowing engineers to fix these vulnerabilities before the product goes to market.
HALT Process:
- Step Stress Testing: Stress levels (such vibration, temperature, or electrical load) are progressively raised in steps during HALT until the product fails. Engineers can determine the precise stress level that leads to failure by holding each step long enough to trigger failure if the product is vulnerable.
- Destructive and Non-Destructive Testing: Both destructive and non-destructive testing methods may be used in HALT. Non-destructive tests find possible failure areas without causing irreversible harm, whereas destructive tests drive the product until it fails.
Figure 22: Constant stress vs. step stress testing
Interpreting HALT Results: The results of HALT provide useful information on the product's design margins and component durability. Understanding the failure modes that occur in high conditions allows engineers to make design changes that improve reliability and ensure that the product can endure its intended operating environment.
Highly Accelerated Stress Screening (HASS)
Highly Accelerated Stress Screening (HASS) is used in production to identify manufacturing flaws and latent problems in individual units, whereas HALT is utilized in the design phase. Similar stress conditions to HALT are used by HASS, but at lower levels, making it appropriate for screening a large variety of products without causing damage.
Implementing HASS:
- Stress Profiles: The data collected during HALT is used to create HASS stress profiles, which guarantee that the screening procedure effectively finds flaws without overstressing the product. Power cycling, vibration, and temperature fluctuations are examples of common stressors.
- Production Line Integration: As a quality control measure, HASS is incorporated into the manufacturing process. While products that fail are further examined to find and fix manufacturing flaws, those that pass HASS are expected to meet their reliability targets in the field.
Benefits of HASS: HASS is an excellent method for lowering the number of early-life failures (infant mortality) by detecting defects before products reach the consumer. This procedure lowers warranty expenditures while increasing overall product reliability.
Failure Modes, Effects, and Criticality Analysis (FMECA)
Failure Modes, Effects, and Criticality Analysis a system is a methodical way to find possible failure mechanisms, evaluate their effects, and rank the priority of corrective measures. All possible reliability issues are addressed during the design and testing phases by using FMECA.
FMECA Process:
- Identify Failure Modes: The initial stage in FMECA is to identify all possible failure modes for each component or subsystem. This comprises mechanical, electrical, thermal, and environmental stresses.
- Assess Effects: Once the failure modes have been determined, the potential implications on the overall system are investigated. This includes assessing how each failure may affect the system's performance, safety, and reliability.
- Criticality Analysis: Criticality analysis ranks failure modes according to their severity, likelihood of occurrence, and detectability. This prioritization allows engineers to focus on the most critical issues that can impact the system's reliability.
Integrating FMECA with Reliability Testing: FMECA is frequently used in tandem with ALT, HALT, and HASS to guarantee that all identified failure modes are fully tested and mitigated. Integrating FMECA into the reliability testing process allows engineers to create more robust designs and ensure that possible issues are addressed before mass production.
Burn-In Testing
Burn-in testing is the process of operating a product under normal or slightly higher stress conditions for an extended period of time before shipping it to customers. The objective is to detect and eradicate early-life failures, often known as "infant mortality" failures, which are usually brought on by manufacturing or material defects.
Burn-In Testing Procedures:
- Temperature and Load Conditions: During burn-in testing, products are exposed to high temperatures, electrical loads, and occasionally vibration. This process accelerates the aging of components, revealing defects that could lead to early failure.
- Duration and Monitoring: The duration of burn-in testing varies according to the product and the anticipated operating conditions. Before the product is issued, engineers may detect faults and take corrective action because of continuous monitoring during burn-in.
Benefits of Burn-In Testing: Burn-in testing enhances overall product reliability by detecting and eliminating early-life issues, as well as lowering the likelihood of failures during the initial phase of field operations.
Environmental Stress Screening (ESS)
A reliability testing technique called environmental stress screening involves subjecting products to conditions that simulate real-world operating conditions. ESS is designed to detect latent defects and manufacturing issues that may result in field failures.
ESS Techniques:
- Thermal Cycling: Thermal cycling is a common technique in ESS that exposes products to alternating high and low temperatures to simulate the impacts of daily or seasonal temperature fluctuations.
- Vibration Testing: Vibration testing simulates the mechanical stresses that products could encounter in mechanically vibrating environments while being transported, installed, or operated.
- Humidity Testing: Products are subjected to high humidity levels during humidity testing in order to evaluate their ability to withstand moisture-related failures, including corrosion or electrical shorts.
Implementing ESS in Production: ESS is often carried out during the manufacturing process, with products tested as individual units or batches. The goal is to eliminate defective products before they are distributed, guaranteeing that only reliable units reach customers.
アカウントにログイン
新しいアカウントを作成