Introduction to HIL Testing
Hardware-in-the-Loop (HIL) simulation is a strong testing methodology that combines real hardware components with a simulated environment to validate complex control systems. By enabling engineers to test control algorithms in real time on real hardware while simulating the rest of the system, this technique bridges the gap between pure software simulations and real-world hardware testing. HIL simulation is frequently utilized in industries such as aerospace, automotive, power electronics, and industrial automation, where safety, reliability, and performance must be thoroughly verified prior to deployment.
Overview of HIL Testing
Combining real hardware with a real-time simulation of the system it interacts with is known as hardware-in-the-loop (HIL) simulation. While the rest of the system, such as the environment or the plant being controlled, is simulated on a high-fidelity digital model, the hardware, such as the controller or sensor, is physically present and functions in real time in this setup. This eliminates the need for the entire physical system to be present and enables realistic testing of control strategies and system behaviors.
How It Works:
HIL systems typically consist of several key components:
Real-Time Simulator: High-fidelity mathematical models of the system, plant, or environment under test are operated by the simulator. For instance, the real-time simulator could simulate a vehicle's dynamics, powertrain, and surroundings in automotive applications.
Physical Hardware: This comprises genuine hardware components that communicate with the real-time simulation, including controllers, sensors, or actuators. Interfaces that simulate real-world connections, such as communication buses or signal conditioning modules, are used to connect the simulator to the physical hardware.
Software Interface: Engineers can use this software to control the simulation, change parameters, and monitor system performance during the HIL test. Engineers can see how the hardware reacts to environmental conditions and simulated inputs.
Real-Time Execution:
The real-time execution of HIL simulation is one of its key features. The simulator receives inputs from the simulated system and provides feedback to the physical hardware, which functions in real-time. Because HIL is real-time, it guarantees that the control algorithms are tested in real-world scenarios where the performance of the system is reflected by time delays, data rates, signal processing, and other constraints.
For example, in a motor control system, the controller hardware may instruct a simulated motor operating in the real-time simulator to compute the motor's response, including torque or speed, and then transmit that information back to the controller.
Importance of HIL in System Testing
Early Validation of Control Algorithms:Engineers can validate hardware and control algorithms early in the development process via HIL simulation, even before the physical system is fully constructed or ready. For instance, in the automobile industry, before constructing a prototype vehicle, engineers can test the engine control unit (ECU) using a simulated engine model. This allows for more rapid identification of potential design issues, lowering development time and costs.
Safe Testing of Critical Systems:Many systems, especially those used in aerospace, automotive, and power electronics, are vital to safety and must be thoroughly tested under a wide range of operating situations. Engineers can replicate extreme conditions (such as maximum load, fault conditions, or environmental extremes) using HIL simulation, which offers a safe environment for testing such systems without endangering physical hardware or raising safety risks. For instance, HIL can be used to evaluate a power inverter for a renewable energy system under various simulated grid conditions and fault scenarios without putting expensive physical assets at risk.
Reduced Development Costs:Physical prototypes of complex systems can be costly and time-consuming to build and test. HIL simulation significantly reduces the requirement for expensive physical prototypes by enabling engineers to test control systems in a virtual environment that closely resembles real-world conditions. Furthermore, HIL lowers the possibility of expensive redesigns or system recalls later in the development cycle by detecting issues in the early design phase.
Testing of Fault Scenarios:With HIL simulation, fault scenarios that could be too dangerous or challenging to replicate with physical hardware can be safely tested. Engineers can model a variety of fault scenarios, including communication glitches, power supply interruptions, and sensor failures, and observe how the control system responds. This increases overall robustness and reliability by guaranteeing that systems are designed to withstand real-world issues.
Examples of HIL in Engineering Applications
Automotive Systems:Electronic control units (ECUs) for advanced driver assistance systems (ADAS), braking systems, transmission control, and engine management are tested using HIL in automotive development. The ECU connects to a real-time simulator that simulates sensor data, engine performance, and vehicle dynamics. Without a physical vehicle, engineers can test how the ECU responds to various driving scenarios, including braking, acceleration, and steering maneuvers.
Power Electronics:HIL simulation is used in power electronics to evaluate motor drives, power converters, and renewable energy systems. A DC/AC inverter, for instance, is tested by connecting its hardware to a simulated grid environment that simulates various voltage levels, grid disruptions, and load variations. This enables engineers to verify the hardware and control algorithms of the inverter and evaluate its performance in a range of grid conditions, including fault scenarios such as over-voltages or voltage sags.
Aerospace Systems:HIL simulation is used in the aerospace industry to verify autonomous navigation, avionics, and flight control systems. A real-time simulator that simulates aircraft dynamics, sensor inputs, and environmental factors including wind turbulence can be used to test a flight control system. Without endangering a real aircraft, engineers can now make sure the control system operates as intended under all conditions, including emergencies.
Summary of Key Benefits
Risk Mitigation: HIL simulation mitigates the dangers associated with testing complex systems by allowing for comprehensive testing in a safe, controlled environment.
Cost Efficiency: HIL allows for faster iteration of control strategies and significantly reduces development costs by eliminating the need for physical system/plant prototypes.
Early Issue Detection: Before the system is completely built, engineers are able to identify and resolve design issues early in the development process using HIL.
Realistic Testing: HIL offers a very realistic testing environment, enabling control systems to interface with simulated real-time hardware and environment conditions.
Advantages of HIL Simulation in Power Conversion Control
Hardware-in-the-Loop (HIL) simulation is an important tool for verifying control systems in real-time scenarios. It provides significant benefits over traditional testing methods in power conversion control, where efficiency, precision, and reliability are crucial. Power conversion systems, including motor drives, inverters, and DC/DC converters, must fulfill strict performance requirements in dynamic and often challenging conditions. HIL simulation provides a controlled, adaptable, and cost-effective platform for testing and optimizing these systems.
Real-Time Validation of Power Conversion Algorithms
The ability to evaluate hardware and control algorithms in real-time is one of the key benefits of HIL simulation in power conversion control. Evaluation of control systems under real-world operating conditions is crucial in power electronics because of the dynamic nature of power converters and the requirement for accurate, fast control. HIL simulation enables engineers to connect real control hardware (such as a digital signal processor or a microcontroller executing control algorithms) to a simulated environment that replicates the power converter's behavior.
In this real-time setup, engineers can test:
Control strategies for stability: Stability is essential in power converters, especially in systems including DC/DC converters and inverters, where sudden load changes and input variances can destabilize the system. HIL enables engineers to model these variations in real time and monitor the performance of the control algorithm and hardware.
Response times and transient behavior: It is essential for power conversion systems to respond quickly to changes in input voltage, load, or fault conditions. Engineers can adjust control parameters to reduce oscillations, overshoot, and undershoot during transients by using HIL simulation to test transient responses in real time.
Safe Testing of Fault Conditions and Edge Cases
To make sure the system operates safely and reliably, power conversion systems must be tested under fault conditions (such as short circuits, overvoltage, or component failures). However, performing these tests on physical systems can be risky, costly, and potentially destructive to the hardware.
Engineers can simulate a wide range of fault conditions using HIL simulation, which offers a secure and regulated environment for fault testing without risking damage to physical equipment. For example, engineers can model the following fault scenarios in the case of an inverter or motor drive:
Sudden load variations: The robustness of the control system can be tested in real-time using HIL simulation, which can simulate rapid changes in load or fault events (such as motor stall or overcurrent conditions).
Grid disturbances: Grid disturbances including voltage sags, frequency fluctuations, or total loss of grid connection can be simulated in real-time using HIL for grid-tied power converters, such as inverters used in renewable energy systems. This enables engineers to verify the control system's ability to initiate a safe shutdown sequence or sustain stable operation.
Engineers can verify protection algorithms, enhance system safety, and make sure the control system can manage the worst-case scenarios without jeopardizing the system's integrity by simulating faults with HIL.
Accelerated Development and Testing
Physical prototypes, which can be expensive and time-consuming to build, are frequently used in traditional power converter designs to validate control algorithms. Furthermore, it might not be possible to test control algorithms early on because the physical system might not be accessible until later in the development phase.
Long before the final physical prototype is built, engineers can test control algorithms on real hardware through HIL simulation, which speeds up the development cycle. Engineers can simulate the power conversion system in real time using a simulator, which allows them to:
Test control strategies early: It is possible to validate and optimize control algorithms parallel with hardware development. Because control algorithms don't have to wait for hardware availability, this drastically cuts down on development time.
Perform iterative testing: Rapid iterations of control algorithm development are made possible by HIL simulation. Without the delays that come with physical prototyping, engineers can immediately adjust the algorithm, conduct testing in real-time, and improve the system as required.
This rapid testing and debugging process enables faster improvement of control strategies, resulting in more efficient power conversion systems at lower development costs.
Flexibility and Scalability in Testing
High degree of flexibility and scalability are provided by HIL simulation, which is especially useful for power conversion systems that need to test a range of control scenarios, configurations, and operating conditions.
HIL systems allow engineers to:
Easily switch between different configurations: Power conversion systems frequently have to function in several configurations or modes (e.g., grid-tied vs. standalone inverters, buck mode, boost mode). Without physically altering hardware configurations, engineers can quickly adapt the simulated system to fit various operating conditions using HIL.
Test a wide range of conditions: To test the control system's performance across its entire operating range and ensure robustness under all conditions, engineers can simulate a wide range of input conditions (such as fluctuating loads, varying input voltages, and temperature variations) and observe how the system responds.
HIL is ideal for testing complex power systems with multiple interconnected stages and varying control strategies, such as modular power converters or multi-level inverters, because of its flexibility. Additionally, it offers scalability because HIL systems can be expanded to incorporate more hardware or simulated subsystems, enabling the testing of large-scale power networks or systems.
Optimization of Power Conversion Efficiency
Power conversion systems are designed to be as efficient as possible, particularly in applications such as industrial automation, electric vehicles, and renewable energy. Small improvements in efficiency can result in considerable cost savings and performance gains. To optimize the control algorithms utilized in these systems, HIL simulation is essential.
Real-time HIL testing allows engineers to:
Fine-tune control parameters: HIL allows for real-time optimization of parameters including duty cycle, switching frequency, and control loop gains to maximize efficiency while preserving response time and stability.
Minimize losses: HIL enables engineers to identify the ideal control settings to reduce losses in power electronics components such as transistors and diodes and evaluate different control strategies, such as maximum power point tracking (MPPT) or pulse-width modulation (PWM) in renewable energy systems.
Reduce heat generation: Engineers can improve the system's overall thermal performance and lifespan by minimizing unnecessary switching losses and heat generation through the optimization of control algorithms using HIL simulation.
Integration with Other Testing Methods
To establish an extensive validation environment, HIL simulation can be effectively combined with other testing techniques such as software-in-the-loop (SIL) and model-in-the-loop (MIL) testing. For instance, in an entirely software-based environment, the control algorithm may be validated early in the development process using MIL and SIL testing. Following the refinement of the control algorithm through these simulations, the algorithm can be tested on physical hardware using HIL.
This integrated testing strategy lowers the potential of performance issues or system failures by ensuring that the control algorithm is rigorously validated at every stage of development.
Implementing Advanced Control Strategies in HIL
Advanced control strategies can be developed, tested, and validated in real-time with the help of hardware-in-the-loop (HIL) testing. HIL simulation allows engineers to assess and improve control algorithms in a safe and controlled environment as they become increasingly complex, especially in industries such as automotive systems, power electronics, and renewable energy. Control strategies that would be difficult, risky, or expensive to test on full physical prototypes can be implemented more easily with HIL's integration of real hardware with a simulated environment.
Overview of Advanced Control Strategies
Advanced control strategies provide more complex, adaptive, and optimal performance in dynamic systems by going beyond traditional linear control techniques such as proportional-integral-derivative (PID) control. These strategies are particularly crucial in power conversion systems, where precise control is necessary for factors such as efficiency optimization, non-linearity, and fast transients.
Some major advanced control strategies are:
Model Predictive Control (MPC): A control strategy that predicts future system behavior and adjusts control actions accordingly.
Adaptive Control: Real-time control parameter adjustments are made to accommodate changing system conditions.
Nonlinear Control: Techniques for managing systems with nonlinear dynamics, such as hysteresis control and sliding mode control (SMC).
Multivariable Control: Manages systems with multiple inputs and outputs while improving performance across all variables simultaneously.
Optimal Control: Attempts to optimize a specific objective, such as reducing energy loss or increasing efficiency.
HIL testing is an effective platform for implementing and evaluating advanced control strategies since it allows engineers to test their real-time performance with physical hardware.
Steps in Implementing Advanced Control Strategies in HIL
When implementing advanced control strategies in an HIL environment, several crucial steps must be taken to guarantee proper real-time interaction between the control algorithm and the physical hardware.
Model Development and System Identification:
Before applying an advanced control approach, it is critical to develop accurate models of the system or plant to be controlled. This step often involves using system identification approaches to generate mathematical models that depict the behavior of the power converter, motor drive, or other controlled systems.
Design and Simulation of the Control Algorithm:
The advanced control algorithm is then designed with tools such as MATLAB/Simulink or other model-based design platforms. Control strategies can be developed and simulated in a virtual environment with the help of these tools.
To verify the control algorithm's fundamental operation, it is tested in a pure simulation environment (model-in-the-loop, followed by software-in-the-loop). Before switching to the HIL platform, engineers can adjust parameters, model various operating conditions, and enhance the algorithm's performance.
Table 10: SIL vs. MIL
| Aspect | Software-in-the-Loop (SIL) | Model-in-the-Loop (MIL) |
|---|---|---|
| Definition | Running the actual software or control code in a simulation environment to validate its behavior and functionality | Using a simulation model of the system (or plant) to test control algorithms or software before integrating it with real hardware |
| Primary Focus | Focuses on verifying and validating the software (control algorithms, code, etc.) before implementation on hardware | Focuses on testing the control algorithm with a model of the system/plant to ensure proper integration and performance |
| System Setup | Involves the actual software running on a simulation platform, interacting with the simulation environment or plant model | Involves a plant model (mathematical or system-level model) running within a simulation tool to test how the control algorithm performs |
| Testing Environment | The control software interacts with simulated input and output signals, simulating real-world conditions and system behavior | The system or plant behavior is simulated using a model, and the control algorithm is tested against this simulated plant |
| Development Stage | Used when the control software is ready, but before hardware integration | Used early in the development process, when the control system is being developed and tested with a model of the plant or system |
Integration with Real-Time Hardware:
Following the simulation of the control strategy, the code is moved to the field-programmable gate array (FPGA) or digital signal processor (DSP), which are examples of the real-time control hardware utilized in the HIL configuration. By interacting with the real-time simulator that simulates the plant or power system, these hardware platforms execute the control algorithm in real-time.
In the integration phase, it is important to make sure that there are no delays or latency in the communication between the control hardware and the simulated system. Real-time processing of the algorithm's control signals is necessary to produce the intended system behavior.
Real-Time Testing and Tuning:
A DC/DC converter, inverter, or motor drive are examples of simulated plants that are used in the HIL environment to test the control strategy in real-time. Variations in load, input voltage, and environmental factors are just a few of the many operational conditions that engineers can introduce.
With HIL, control parameters can be quickly adjusted in response to real-time performance data. Engineers can observe how the advanced control strategy responds to the system's nonlinearities, disturbances, and dynamic conditions. To guarantee that the control strategy operates optimally across a variety of conditions, fine-tuning is necessary.
Fault Testing and Stress Conditions:
Testing in fault conditions is an additional advantage of HIL simulation, which is crucial for advanced control strategies that are needed to guarantee system safety and reliability. Engineers can test how the control algorithm responds by introducing faults such as overvoltage, short circuits, or grid disturbances.
Fault detection and mitigation capabilities, such as switching to a backup control mode or safely shutting down the system, are frequently included in advanced control strategies. These crucial functionalities can be tested in a risk-free environment with HIL simulation.
Optimization for Real-World Implementation:
Once the control algorithm has proven effective in the HIL environment, the next step is to improve it for real-world deployment. This includes ensuring that the control strategy will execute efficiently on the target hardware, with considerations for real-time execution, processing power, and memory utilization.
HIL offers the optimal platform for determining whether the control strategy can be implemented on production-grade hardware while guaranteeing that the algorithm satisfies the required resource and performance limitations.
Examples of Advanced Control Strategies in HIL
Model Predictive Control (MPC) for Power Converters:MPC is used in power electronics to forecast the converter's future states and optimize switching actions to reduce losses and enhance dynamic response. Engineers can test MPC's performance in real-world operating conditions and optimize its predictive model in real-time by implementing it in an HIL environment.
Nonlinear Control for Motor Drives:Motor drives frequently employ nonlinear control strategies, such as hysteresis control or sliding mode control, to manage system nonlinearities. Real-time testing of these strategies is made possible by HIL simulation, which guarantees that the control algorithm can continue to function and remain stable in spite of changes in speed or load.
Adaptive Control in Renewable Energy Systems:Renewable energy systems including solar inverters and wind turbines frequently use adaptive control algorithms, which modify control parameters in response to changing system conditions. Real-time validation of these algorithms is made possible by HIL testing, which guarantees that they can adjust to variations in load, weather, or grid disruptions.
Practical Considerations
Hardware-in-the-Loop (HIL) simulation is a robust tool for real-time testing and validation of complex control systems, but its optimal implementation necessitates meticulous planning and attention to a number of practical considerations. These considerations encompass a variety of areas, such as cost management, real-time performance, hardware selection, integration challenges, and system safety. Effectively addressing these issues guarantees that the HIL system operates at peak efficiency and that test results accurately depict real-world conditions.
Selection of Appropriate Hardware
Real-Time Processors and Controllers:
For any HIL system, its ability to execute simulations in real time without lag or delay is the most important requirement. The processors and controllers utilized in the HIL setup must be selected based on the computational complexity of the models being simulated as well as the speed with which control loops must be executed.
To guarantee that the simulations can operate at the necessary speed, multi-core processors, field-programmable gate arrays (FPGAs), and high-performance digital signal processors (DSPs) are frequently used. To ensure accurate real-time testing, the control algorithms must execute faster than the plant's dynamics.
For instance, the HIL system must process control signals and feedback in real time to provide meaningful results in a power electronics system where switching times in the microsecond range.
Communication Interfaces:
Controllers, sensors, and actuators are examples of hardware components that must interface seamlessly with the simulation platform during HIL testing. Proper communication interface selection (e.g., CAN, Ethernet, SPI, I2C) is critical for ensuring low-latency and high-speed data flow between the simulated system and the physical hardware.
Errors in the system's real-time behavior can be introduced by any delays in signal transmission between the simulator and the control hardware. Therefore, depending on the system's performance requirements, high-bandwidth and real-time communication interfaces should be selected.
System Latency and Real-Time Constraints
Minimizing Latency:
The ability of an HIL setup to replicate real-world system dynamics without introducing noticeable delays (latency) is one of the main criteria that determines its success. Even a small delay can have an impact on the control algorithm's response fidelity in real-time systems.
The system's overall latency, which can result from data processing, signal transmission, or insufficient processing power, must be reduced to a minimum. Maintaining low latency requires that the software, I/O interfaces, and processor be optimized for real-time execution.
Real-Time Operating Systems (RTOS):
The HIL system should run on a real-time operating system (RTOS) to guarantee that operations such as control computation and signal acquisition are completed within the required time limits. Deterministic timing, which is necessary for tasks where timing predictability is crucial, is provided by RTOS.
The RTOS ensures that high-priority operations, such as control algorithm execution or feedback acquisition, are completed without delay, minimizing the influence on system performance.
Table 11: RTOS functions
| Aspect | Real-Time Operating System (RTOS) Uses in HIL |
|---|---|
| Definition | RTOS is an operating system designed to process real-time applications that require consistent and predictable responses to events |
| Purpose in HIL | RTOS is used in HIL to ensure that the system’s hardware components and software models interact with real-time constraints effectively |
| Real-Time Processing | RTOS ensures that critical tasks (e.g., sensor data processing, control algorithm execution) are processed within strict timing requirements, crucial for accurate HIL simulation |
| Task Prioritization | RTOS provides task prioritization mechanisms to manage multiple real-time tasks in HIL simulation, ensuring high-priority tasks (e.g., control loops) are executed first |
| Latency Control | RTOS minimizes latency between sensor inputs and actuator outputs, crucial in HIL to simulate the real-world response of a system accurately and in real-time |
| Interrupt Handling | RTOS handles interrupts efficiently, ensuring quick responses to external signals (such as sensor data changes) in the HIL setup, allowing immediate action based on the hardware state |
| Resource Management | RTOS manages system resources like CPU, memory, and I/O devices, ensuring that the computational load in HIL simulation does not exceed system limits and tasks are completed on time |
| Synchronization | RTOS provides synchronization tools like semaphores and message queues, which help coordinate between real-time tasks and hardware in HIL testing |
| Data Acquisition and Processing | RTOS ensures that real-time data acquisition from hardware interfaces (sensors, actuators) and processing of this data (control laws, algorithms) occur with minimal delays |
Synchronization of Hardware and Simulation:
It's crucial that the simulated system and the physical hardware are properly synchronized. Inaccurate test results or even system instability may arise from timing discrepancies between the simulation environment and the control hardware.
Engineers must carefully calibrate the timing in the HIL configuration to guarantee that the control signals given by the physical hardware are applied to the simulated plant at the correct time.
Scalability and Flexibility
Scalability of HIL Systems:
Scalability must be considered in the design of HIL systems, particularly when testing complex systems such as electric vehicle platforms, power grids, or renewable energy systems. The HIL environment should be able to support additional hardware components, subsystems, or control algorithms as the system being tested evolves or expands without requiring a complete redesign.
For instance, while testing a solar inverter's power electronics, the HIL system should be able to scale to simulate load conditions, grid connections, battery storage, and the inverter itself.
Modular HIL Platforms:
Many modern HIL systems are modular, which means that new hardware or software components can be added as needed. Because of its modularity, engineers can reuse the same HIL platform across projects with minimal changes, providing them with flexibility.
For example, by adding or removing the relevant models and hardware interfaces, the same platform can be used to test different subsystems in an automotive HIL system, such as engine control, braking, or battery management.
Safety and Fault Testing
Testing Safety-Critical Systems:
Safety is a major concern in several industries, including power electronics, automotive, and aerospace. With HIL simulation, safety-critical control systems can be safely tested in real-world scenarios without endangering real physical systems. HIL systems should have safety procedures to avoid unwanted outcomes or damage during testing. For instance, the HIL system should be able to safely stop the simulation or identify the issue without harming the physical hardware if the control system being tested sends incorrect commands.
Fault Injection and Testing:
The response of a system to fault conditions, such as sensor failures, short circuits, or unexpected disruptions, is frequently assessed via HIL testing. Engineers can test how successfully the control system detects and mitigates defects by simulating them in a controlled environment.
Fault testing necessitates meticulous planning to guarantee that the system is not accidentally destroyed during the test. HIL systems should include built-in fault protection techniques, such as overcurrent or overvoltage protection, to protect both the hardware and the simulated environment under these extreme conditions.
Cost and Resource Considerations
Cost of HIL Systems:
It can be costly to implement a complete HIL setup, especially when dealing with complex, large-scale systems. In addition to the hardware (processors, I/O interfaces, controllers), the cost additionally includes software licenses for RTOS platforms and real-time simulators.
To justify the investment, HIL systems should be employed in applications where the prospective cost reductions (such as reduced prototype development, fewer hardware failures, and faster time to market) outweigh the initial expenditures.
Resource Allocation:
In HIL testing, engineers must balance memory, processing power, and I/O bandwidth between the control hardware and the real-time simulation; executing simulations that are too complicated for the hardware at hand may result in slowdowns or incorrect results.
To ensure the HIL system operates as efficiently as possible during testing, resource utilization must be closely monitored. To fit within the system's constraints, it may be necessary to reduce the fidelity of the model or use more optimized algorithms.
Verification and Validation Procedures
Model Validation:
In HIL testing, ensuring the simulated models accurately depict the real system is one of the fundamental challenges. The models used to simulate the plant, power converter, or other components must be verified against actual physical data prior to the implementation of HIL.
To increase accuracy, model validation usually includes comparing the HIL simulation's output with measurements from the real system and modifying the model's parameters as needed.
Test Repeatability and Documentation:
Results from HIL testing should be consistent and repeatable. Engineers must verify that test cases are clearly documented and can be executed consistently over multiple test runs. Test findings must be properly documented in order to troubleshoot issues, improve the control algorithm, or demonstrate regulatory compliance.
Furthermore, engineers should use automation tools found in modern HIL platforms to automate test sequences and data collecting, guaranteeing that tests can be repeated consistently.
Integration with Other Development Tools
Compatibility with Design and Simulation Software:
The software tools used in the design phase, including MATLAB/Simulink, LabVIEW, or SPICE, must be easily integrated with HIL systems. Because of this interaction, engineers may easily switch from software-in-the-loop (SIL) and model-in-the-loop (MIL) testing to HIL testing.
Models, control algorithms, and test scripts can be exported directly from design software to the HIL platform, streamlining the process and facilitating faster development cycles.
Continuous Development and Testing:
Continuous integration and testing environments, where control algorithms are updated frequently and new test cases are added, are perfect for HIL systems. Engineers can guarantee new control strategies are evaluated in real-time with real hardware during the development process by including HIL in a continuous development pipeline.
Log in to your account
Create New Account