Watchdog Timers
Session textval
Session Titefor popup
MPS’s automotive watchdog timers achieve system stability by supervising a timing signal from a processor or MCU to ensure proper operation.
Watchdog Timers Content
-
ARTICLE
フライバックコンバータの電圧スパイクを抑制するソリューション寄稿文フライバックコンバータトポロジーは、低電力の絶縁型電源で採用されている最も一般的なトポロジーの一つです。フライバックコンバータの成功の鍵は、昇降圧インダクタンスをトランスの2つの巻線に分割できることにあり、これにより柔軟な電圧比と電流比を実現できるだけでなく、絶縁という利点も得られます。その結果、フライバックコンバータは必要な部品点数が少なく、広い動作幅にわたって安定した性能を発揮します。 しかし、トランスの漏れインダクタンスに蓄積されたエネルギーによって重大な電圧スパイクが発生し、フライバックコンバータの設計において共通の課題となっています。電圧スパイクが定格電圧を超えると、電源スイッチに損傷を与える可能性があります。電圧スパイクによって引き起こされる二次的な問題は、高周波の高調波を発生させる電磁障害 (EMI) です。 従来の手法では、漏洩エネルギーを吸収し、スパイ...
-
ARTICLE
AN EQUATION-DRIVEN GUIDE TO DESIGNING A CRM/DCM BOOST PFC寄稿文Designing compact and efficient power factor correction (PFC) stages for low-power to mid-power applications often requires operating in critical conduction mode (CrM) or discontinuous conduction mode (DCM). These modes offer improved efficiency and simplified control at light loads, but require careful design to ensure correct valley detection and mode transitions across the entire input range an...
-
VIDEO
WEBINAR - INSIDE AUTOMOTIVE DMS & OMSビデオExplore DMS/OMS fundamentals, focusing on typical system architecture, camera power architecture, and the use of MPS IR LED drivers to manage high peak currents and thermal performance in automotive imaging systems. The webinar also covers camera placement and the evolution of the smart cockpit. Key takeaways include: System & Power Architecture: Master the complete system and power architect...
-
ARTICLE
THE THEORY OF PARASITIC MILLER TURN-ON AND DRIVING TECHNIQUES FOR SIC MOSFETS AND CASCODES寄稿文To address the constant challenges that accompany increasing a power converter’s power density, switching frequency (fSW), and efficiency, it is vital that designers can switch power transistors quickly and safely. These needs have made wide-bandgap power semiconductors like silicon carbide (SiC) MOSFETs and cascodes more popular than silicon counterparts; however, these devices also work at much ...
-
ARTICLE
AIサーバーアプリケーション向けピーク電力削減ソリューションの設計寄稿文AIシステムの急速な発展により、AIサーバの電力要件は進化しています。AIトレーニングが開始されると、AIの電力需要は、GPUのアイドル状態の電力の10倍を超える電力が一気に必要となる可能性があります。これらの電力の急激な増加により、サーバーの電源装置 (PSU) で大きな突入電流が発生したり、PSUが過負荷になったりすることがあります。 ただし、ほとんどのAIトレーニング期間は比較的短時間であり、その後、GPUははるかに長い期間アイドル状態のままになります。そのため、こうした短い電力増加は、サーバー電源システムのピーク能力を超えることがありますが、平均電力要件を大幅に変化をもたらすことはありません。高出力PSUモジュールは、このピーク電力要件を満たしますが、コスト効率が低く、より多くのシェルフスペースを必要とします。 このことを念頭に置くと、新しいAIサーバーのPSUでは、P...
-
ARTICLE
DRIVING THE TOTEM-POLE CONVERTER'S SLOW LEG WITH RELIABILITY寄稿文Whether traditional or cutting-edge, most high-voltage power converter topologies are comprised of transistors placed either in half-bridge or full-bridge combinations. Typically, a bootstrap technique is used to drive the high-side transistor when a negative voltage is not required for the gate. While this technique seems simple and straightforward, special care must be taken when dealing with AC...
-
ARTICLE
AI-POWERED ROBOTICS NEED ADVANCED SOC SOLUTIONS寄稿文The robotics industry is undergoing a major transformation driven by advancements in artificial intelligence (AI), machine learning, and real-time data processing. Today, AI-powered robots are transforming the future of robotics by making systems smarter, more adaptive, and more autonomous. Autonomous robots that were once a topic of futuristic writing are heading for mass production today. Human...
-
ARTICLE
PFC導通モードを選択するための4ステップガイド: CRM / DCM VS. CCM寄稿文力率補正 (PFC) 昇圧型コンバータは、IEC 61000-3-2などの高調波電流規制を満たすための産業標準トポロジーです。この回路は、現代のAC/DC電源において不可欠であり、入力電圧 (VIN) 正弦波形に従うように入力電流(IIN)を整形し、1に近い力率を達成します。 PFC設計を成功させる鍵は、その動作モードにあります。連続導通モード (CCM)、不連続導通モード (DCM)、臨界導通モード (CrM) という3つの基本モードが存在しますが、根本的な設計上の選択は、CCM向けに構築されたシステムとCrM向けに最適化されたシステムのどちらを選択するかという点にあります。CrM用に設計されたコントローラは、負荷が軽い場合には自然とDCMで動作するため、CrMとDCMは多くの場合、単一の設計経路 (CrM / DCM) としてまとめて解析されます。 CCMとCrM / DCMのどち...
-
APPLICATION
AI用ハードウェアアプリケーション -
ARTICLE
UNDERSTANDING ACCURACY AND RESOLUTION FOR MAGNETIC ANGLE SENSORS寄稿文Magnetic position sensors, especially magnetic angle sensors, are the fundamental building blocks of countless motion-control applications that necessitate precision positioning. These sensors are pivotal in a wide range of industries, from automotive and robotics to consumer electronics and medical devices, underscoring their universal appeal and importance (see Figure 1). However, to ...
-
ARTICLE
自動車革命の推進: ゾーンアーキテクチャから48Vへ寄稿文自動車産業は、大規模な変革の真っ只中にあります。過去10年間で、自動車には顧客により高い安全性、快適性、使いやすさ、そして楽しさを提供する先進的な機能がますます搭載されるようになってきています。それには、シートヒーターからインフォテインメント用スクリーン、安全カメラ、ハイエンドのサウンドシステムまで、あらゆるものが含まれます。最も革新的な乗り物の中には、完全自動運転車やロボットタクシーなどがあります。 こうした最先端の運転体験向上機能はすべて、電力を必要とします。それも相当な電力です。これはつまり、過去70年間自動車業界を支配してきた従来の12Vシステムを、必要な高レベルの電力を供給するために48Vに変更する必要があるということです。しかし、この大きな変革を実現するためには、産業はまず簡素化され、合理化されたゾーンアーキテクチャを採用する必要があります。 電子制御ユニット ...
-
ARTICLE
SOLID-STATE RELAYS FOR THERMOSTAT DESIGN寄稿文The relay is the most failure-prone component in a residential thermostat. Mechanical relays wear out, generate audible noise, produce electromagnetic interference (EMI), and consume valuable printed circuit board (PCB) area. For engineering teams designing the next generation of smart thermostats, these limitations directly impact product lifespan, certification timelines, and field failure rates...
アカウントにログイン
新しいアカウントを作成