Today’s datacenters use a lateral power delivery system, in which the power voltage regulators are
placed on the top side of the board around the processor. As the current demand of CPUs and GPUs
increases, the distance between the voltage regulator and the point-of-load (PoL) becomes a significant
factor for power delivery network (PDN) losses. In addition, increased PDN means that the system requires a large amount
of output capacitance for the voltage regulators.
Z-Axis Power DeliveryTM is a method by which the voltage regulators are placed on the bottom side of
the PCB below the processors. This results in a significant reduction (more than 10X) in PDN losses.
Lateral Power Delivery <1000A
Z-Axis Power DeliveryTM >1000A
MPS offers power module solutions with <4mm height to fit in the limited space on the bottom side of the PCB.
アカウントにログイン
新しいアカウントを作成