AC-DC converters have numerous applications across various industries and systems, including electronic devices, home appliances, automotive systems, power distribution systems, and renewable energy systems. They are primarily used to convert AC voltage into DC voltage, making it possible to power DC devices and store energy in batteries.
Renewable energy systems, such as solar panels and wind turbines, generate AC power that requires conversion to DC power before it can be used by the load or stored in batteries. AC-DC converters are integral to this process, ensuring that the output voltage is stable and appropriate for the load or battery.
Another application of AC-DC converters is in uninterruptible power supplies (UPS). In a power outage, the UPS uses a battery to provide a continuous DC power source to the load. To ensure the battery is charged and the power supply is efficient, AC-DC converters are used to convert the AC voltage from the primary power source into DC voltage.
AC-DC converters also have an important application in industrial and commercial applications where DC motor drives are widely used. These converters are necessary to convert the AC voltage into a DC voltage that the motor can use.
Conclusion
AC-DC converters are crucial for the efficient and dependable operation of power electronics systems in various industries and applications. They are responsible for maintaining a steady output voltage, efficient power transfer, and delivering the required power to DC loads or batteries. As a result, AC-DC converters are an essential component of many electronic systems and industries.
Related Content
-
ARTICLE
HOW TO DESIGN A HALF-BRIDGE LLC RESONANT CONVERTER WITH A CENTER-TAPPED TRANSFORMERARTICLELLC resonant converters have become a cornerstone in power electronics, and widely adopted across various markets due to their ability to achieve high efficiency while minimizing electromagnetic interference (EMI) through soft-switching techniques. LLC topology offers several configurations optimized for specific applications. In particular, there are two prominent configurations for the primary s...
-
ARTICLE
OPTIMIZING HOME REMOTE CONTROLS WITH MPS PRODUCTSARTICLEInfrared (IR) and remote frequency (RF) home remote controls are being used in systems such as sound systems, televisions, lighting, and other controls. These systems are becoming increasingly complex with features including voice control, connectivity, LED displays, and capacitive touch. Remote controls should be reliable, easy to use, and have a long battery lifespan. MPS provides cost-effectiv...
-
ARTICLE
AN INTRODUCTION TO FLYBACK CONVERTERS: PARAMETERS, TOPOLOGY, AND CONTROLLERSARTICLEFlyback converters are versatile power electronics devices used in applications such as medical devices and laptops. Also known as isolated buck-boost converters, these converters are simple circuits that can regulate a system’s output voltage (VOUT) while minimizing electromagnetic interference (EMI). This article will introduce flyback converters, and explore their topology, useful parameters, ...
-
ARTICLE
DESIGNING MULTIPLE INDEPENDENT AUXILIARY POWER SUPPLIES WITH MAGNETIC ISOLATIONARTICLEIn a DC/DC converter, the auxiliary power supply of multiple switching devices requires independent isolated power supplies. Taking a full-bridge converter as an example, the high-side and low-side MOSFETs (HS-FETs and LS-FETs, respectively) of the bridge arm require isolated power supplies for the gate driver circuit. The traditional scheme uses a bootstrap circuit to power supply both the upper ...
-
ARTICLE
ADVANCING THE SYNCHRONOUS RECTIFIER FOR NEW FLYBACK CONVERTERSARTICLEFlyback topology has dominated low-power AC/DC applications for decades due to its simplicity and robustness across a wide operating range. In recent years, synchronous rectifiers (SRs) have replaced the conventional Schottky diode in flyback-based power supplies to significantly improve efficiency. As the demand for efficiency and power density increases year by year, flyback converters must con...
-
ARTICLE
FEASIBILITY AND ACCURACY ANALYSIS OF INPUT POWER ESTIMATIONARTICLEPFC converters are widely used in the industry to provide DC output voltage from the main lines, and to maintain a high power factor (PF) and low current distortion at the same time. In some of these applications, such as telecom, server, workstation power supplies, and plug-in electric vehicles, the active input power needs to be measured in real time in order to monitor energy consumption, as we...
-
ARTICLE
MEASURING HIGH-FREQUENCY, COMMON-MODE CURRENT, VOLTAGE, AND IMPEDANCE (PART III)ARTICLEThis is the final part of a three-part series discussing measurement methods for high-frequency, common-mode (CM) current, voltage, and impedance using a flyback converter. Part I covered the basic principles of radiated EMI and the traditional method for measuring CM current in a flyback converter topology. Part II explored a ferrite bead solution for CM current measurement errors and how to obta...
-
ARTICLE
MEASURING HIGH-FREQUENCY, COMMON-MODE CURRENT, VOLTAGE, AND IMPEDANCE (PART II)ARTICLEThis is the second part of a three-part series discussing measurement methods for high-frequency, common-mode (CM) current, voltage, and impedance using a flyback converter. Part I covered the basics of radiated EMI and the traditional method for measuring CM current in a flyback converter topology. Part II will propose a solution to common errors when measuring CM current, and then it will demons...
-
ARTICLE
TRANSFORMING THE LOW-CARBON ERA WITH MPS'S AC/DC POWER SOLUTIONS (PART II)ARTICLETo meet the increasingly stringent requirements for environmentally friendly solutions, MPS’s AC/DC power supply products utilize advanced technologies to enhance performance and achieve energy conservation. This article is the second in a two-part series to discuss trend-setting AC/DC solutions. Part I served as an introduction for the carbon-free era and the problems that designers face with tr...
-
ARTICLE
DEVELOPING A MULTI-PORT FAST-CHARGE SOLUTION WITH THE HR1211ARTICLEThe HR1211 is an integrated, multi-mode PFC and current mode LLC controller solution that was designed to meet the power requirements of the fast-charge adapter market. To achieve a simplified peripheral circuit, the HR1211 integrates a high-voltage current source, a safety-certified X-capacitor discharge circuit, and high-voltage drive circuits for PFC and LLC. In addition, a capacitor resistor i...
-
ARTICLE
MEASURING HIGH-FREQUENCY, COMMON-MODE CURRENT, VOLTAGE, AND IMPEDANCE (PART I)ARTICLETo obtain an accurate EMI analysis when modeling power electronics, it is crucial to measure the impedance on the noise source and propagation path. For radiated EMI, the corresponding frequency band is typically between 30MHz and 1GHz. Due to the high frequency, it can be difficult to measure parameters such as voltage, current, and impedance. This article is the first part of a three-part serie...
-
ARTICLE
GENERATING AND TESTING POWER RIPPLESARTICLEThe magnitude of power ripples is a common parameter to consider when designing a power supply. As a result, ripples are widely used in testing projects for power engineers. This article will discuss how power ripples are created, and how they can be tested. Note that in this article, “power ripple” specifically refers to the AC component on a power supply’s output, which has a DC voltage. Because...
Log in to your account
Create New Account