Thermostat
Session textval
Session Titefor popup
Thermostat Content
Description
Block Diagram
Select parts to expand information in chart below
Components List
Resources
-
ARTICLE
SOLID-STATE RELAYS FOR THERMOSTAT DESIGNARTICLEThe relay is the most failure-prone component in a residential thermostat. Mechanical relays wear out, generate audible noise, produce electromagnetic interference (EMI), and consume valuable printed circuit board (PCB) area. For engineering teams designing the next generation of smart thermostats, these limitations directly impact product lifespan, certification timelines, and field failure rates...
-
PRODUCT
MP27931PRODUCT5kVRMS, Quad-Channel Digital Isolator with 3 Forward Channels and 1 Reverse Channel
-
PRODUCT
MP9566PRODUCTCompact and Robust 24V AC Switch with I2C/EN Interface
-
PRODUCT
MP28600PRODUCTUltra-Low 600nA Quiescent Current, Down to 0.1V VIN, Synchronous Boost Converter
-
PRODUCT
MP3320BPRODUCT4-Channel, Synchronous Boost RGBW LED Driver with Digital Interface
-
PRODUCT
MP3320APRODUCT4-Channel, Charge Pump RGB LED Driver with Digital Interface
-
PRODUCT
MP3326PRODUCT16-Channel,50mA/Ch,LEDDriver withSeparate PWMAnalog DimmingandI2CInterface
-
PRODUCT
MP3362PRODUCTSingle-String, 3V Minimum VIN, 36V VOUT, Boost LED Driver
-
PRODUCT
MIE1W0505BGLVHPRODUCT5V, 1W, Regulated, 2.5kVRMS Isolated DC/DC Module
-
PRODUCT
MP3370PRODUCTSingle String, 38V Vout Boost LED Driver with Current Source
-
PRODUCT
MPQ27831PRODUCT3kVRMS 2- to 4-Channel Digital Isolator with Integrated Isolated Power Supply
-
PRODUCT CATEGORY
SOLID STATE RELAYPRODUCT CATEGORY -
PRODUCT CATEGORY
RGB LED DRIVERSPRODUCT CATEGORY -
ARTICLE
AN INTRODUCTION TO MPS’S BOOST, BUCK, AND BUCK-BOOST CONVERTERSARTICLEConverters are one of the most simplistic and necessary devices in modern electronics. As their name implies, converters are meant to convert a given value to a target value. This functionality is vital for any system where connected devices may not have specifications that perfectly match one another, and they can be implemented in smartphones, smart trackers that can quickly communicate location...
-
ARTICLE
MIE1W0505BGLVH AWARDED ANNUAL POWER MANAGEMENT/VOLTAGE CONVERTER PRODUCTARTICLEThe 2024 World Electronics Achievement Awards ceremony was held in Shenzhen, China on November 5 by AspenCore, a renowned media group in the global electronics technology field. The MIE1W0505BGLVH, MPS’s ultra-small, isolated power module, won the “Annual Power Management/Voltage Converter Product” award (see Figure 1). The various awards in the World Electronics Achievement Awards ceremony...
-
ARTICLE
HOW TO APPLY AN ISOLATED POWER MODULE IN SIGNAL ISOLATIONARTICLESignal transmissions are everywhere. In industrial applications, such as electric vehicle (EV) charging stations and automation systems with programmable logic controllers (PLCs), there is a high voltage (up to several kV) that can be dangerous to the human body. This type of hazardous voltage can also pass through the signal line, which can cause signal interference and could eventually destroy t...
-
USE CASE
POWER MANAGEMENT USE CASE: E-BIKESUSE CASEThis use case examines the application of the MP4581, MP27631, MIE1W0505BGLVH, and MP5042 in the design of e-bikes. MPS offers strategic power management solutions with the MP4581, MP27631, MIE1W0505BGLVH, and MP5042 to improve battery life and reliability in e-bike systems. Efficient power management is crucial for e-bikes, which are comprised of a rechargeable battery system, a con...
-
USE CASE
POWER MANAGEMENT USE CASE: POWER METERSUSE CASEThis use case examines the application of the MP5493, MP5042, and MIE1W0505BGLVH in power meters. MPS provides the MP5493, MP5042, and MIE1W0505BGLVH to control power surges, voltage transients, and sudden power outages in power meters. Power meters measure key parameters of electrical power consumption in residential and commercial buildings, energy systems, manufacturing, and charging infr...
-
APPLICATION
LOW-VOLTAGE ENERGY STORAGEAPPLICATIONA low-voltage, battery-based energy storage system (ESS) stores electrical energy to be used as a power source in the event of a power outage, and as an alternative to purchasing energy from a utility company. Having an ESS allows homeowners to store excess solar-generated electricity, providing flexibility in when they buy and sell electricity to the utility company, leading to significant cost s...
-
PRODUCT CATEGORY
RGB LED DRIVERSPRODUCT CATEGORY -
APPLICATION
ONBOARD CHARGING MODULE (OBCM)APPLICATIONElectric vehicles (EVs) are becoming more present every day, with the adoption of EVs growing at an exponential rate. Onboard charging (OBC) is a very important part of EVs, since it determines the maximum possible charge rate while an AC charger is connected to the vehicle. The maximum charge capability for a fully electric vehicle is typically between 6.6kW and 22kW, and for a plug-in hybrid veh...
-
APPLICATION
DC FAST CHARGING STATIONAPPLICATIONDC fast charging stations are becoming more common with the increased adoption of electric vehicles. Charging stations are a vital part of the infrastructure along major highways and populated suburbs, ensuring that electric vehicles have a place to charge during long-distance travel and day-to-day driving. These systems are often comprised of multiple 25kW to 75kW modules to create fast charging ...
-
ARTICLE
MPS POWER MANAGEMENT SOLUTIONS FOR POWER OVER ETHERNET (POE) SWITCHESARTICLEModern devices are increasingly powered by Power over Ethernet (PoE), such as IP phones, wireless APs, and IP cameras. Customer premise equipment (CPE) and small base stations in the 5G era also require PoE power. Figure 1 shows common applications powered by PoE. This article discusses MPS’s comprehensive suite of power management solutions for a wide range of switches, including PSE, boo...
-
APPLICATION
PROGRAMMABLE LOGIC CONTROLLER (PLC)APPLICATION -
PRODUCT CATEGORY
DIGITAL ISOLATORSPRODUCT CATEGORY
Log in to your account
Create New Account