Converters
Session textval
Session Titefor popup
saving board space and cost
with low noise
BCD process, &
packaging technology
Converters Content
-
ARTICLE
PRACTICAL DESIGN OF A MULTI-OUTPUT FLYBACK CONVERTER WITH IMPROVED CROSS-REGULATIONARTICLEA stacked-output topology, combined with a weighted feedback network, improves cross-regulation in multi-output flyback converters. This approach allows the main regulated output and the stacked auxiliary output to both contribute to the feedback loop, reducing the voltage deviation typically observed in semi-regulated flyback outputs. This article applies that methodology to a complete offline...
-
ARTICLE
MEETING THE IMPEDANCE MASK: STRATEGIES FOR PDN DESIGN AND OPTIMIZATIONARTICLEIn telecommunication applications, target impedance serves as a crucial benchmark for PDN design. It ensures that the die operates within an acceptable level of rail voltage noise, even under the worst-case transient current scenarios, by defining the maximum allowable PDN impedance for the power rail on the die. This article will focus on the optimization techniques to meet the target impedance ...
-
ARTICLE
OPTIMIZING HOME REMOTE CONTROLS WITH MPS PRODUCTSARTICLEInfrared (IR) and remote frequency (RF) home remote controls are being used in systems such as sound systems, televisions, lighting, and other controls. These systems are becoming increasingly complex with features including voice control, connectivity, LED displays, and capacitive touch. Remote controls should be reliable, easy to use, and have a long battery lifespan. MPS provides cost-effectiv...
-
ARTICLE
IS DESIGN REUSE A MYTH FOR ANALOG CIRCUITS?ARTICLEI have been invited to comment on electronic design automation (EDA). It is a subject in the industry to which I have not contributed much innovation, but I can say a few words as someone who has benefited from it during my long career as an analog designer. With just over 25 years of experience designing DC/DC power converters as well as custom and standard analog IC products, I have seen some r...
-
ARTICLE
PREDICTIVE TRANSIENT SIMULATION ANALYSIS FOR THE NEXT GENERATION OF GPUSARTICLENowadays, graphics processing units (GPUs) feature tens of billions of transistors. With each new generation of GPUs, the number of transistors in GPUs continues to increase to improve processor performance. However, the growing number of transistors is also resulting in an exponential increase in power demand, which makes it more difficult to meet transient response specifications. This article ...
-
ARTICLE
HOW TO CALCULATE A BUCK CONVERTER'S INDUCTANCEARTICLEIn the buck circuit, the inductor design is a key element that is closely related to system efficiency, the output voltage ripple (∆VOUT), and loop stability. This article discusses how to calculate the inductance of a buck converter using the MPQ2314 as well as key parameters including the rising current of the inductor temperature, saturation current DC resistance, operating frequency, and magne...
-
ARTICLE
PLANNING FOR SUDDEN POWER FAILURES WITH THE MP5515ARTICLEPower failures tend to cause a domino effect of disruptions, resulting in system failures and data loss, as well as damage to servers and equipment. This article describes how to use the MP5515 to protect solid-state drives (SSDs) against sudden power failure. There are three main issues if an SSD experiences a power failure: The MP5515 is an input power conditioning PMIC that provides a compact...
-
REFERENCE DESIGN
VERSAL HBM – FULL POWER MANAGEMENT DEVICE (OPTIMIZED FOR EFFICIENCY)REFERENCE DESIGN -
REFERENCE DESIGN
VERSAL HBM – M/H DEVICE (OPTIMIZED FOR EFFICIENCY)REFERENCE DESIGN -
REFERENCE DESIGN
VERSAL HBM – L DEVICE (OPTIMIZED FOR EFFICIENCY)REFERENCE DESIGN -
REFERENCE DESIGN
VERSAL AI EDGE – FULL POWER MANAGEMENT (OPTIMIZED FOR EFFICIENCY) -L DEVICESREFERENCE DESIGN -
REFERENCE DESIGN
VERSAL AI EDGE –M/H DEVICE (OPTIMIZED FOR EFFICIENCY)REFERENCE DESIGN
Log in to your account
Create New Account