Session textval
Session Titefor popup
Molded Inductors for MPS Products
This series includes molded magnetic-shielded power inductors that offer soft saturation due to their molded design, delivering a stable high-temperature behavior. Their molded construction decreases the audible noise generated from alternating currents and pulse wave frequencies.
Inductor Selector Tool
Molded Optimized for MPS DC DC Content
-
ARTICLE
DESIGNING A PEAK POWER-SHAVING SOLUTION FOR AI SERVER APPLICATIONSARTICLEThe power requirements of AI servers are evolving due to the rapid development of AI systems. When AI training starts, the AI GPU power demands can require short bursts of power that exceed the GPU’s idle-state power by 10 times. These power bursts can cause a large inrush current at the server’s power supply units (PSUs) or even overload the PSUs. However, most AI training periods last for a r...
-
ARTICLE
A SIMPLE, EFFECTIVE SOLUTION TO SUPPRESS VOLTAGE SPIKES IN FLYBACK CONVERTERSARTICLEFlyback converter topology is one of the most popular topologies adopted by low-power, isolated power supplies. The key to the flyback converter’s success is the ability to divide the buck-boost inductance into two windings of a transformer, creating flexible voltage and current ratios with the additional advantage of isolation. As a result, flyback converters require few components and achieve ro...
-
ARTICLE
AI-POWERED ROBOTICS NEED ADVANCED SOC SOLUTIONSARTICLEThe robotics industry is undergoing a major transformation driven by advancements in artificial intelligence (AI), machine learning, and real-time data processing. Today, AI-powered robots are transforming the future of robotics by making systems smarter, more adaptive, and more autonomous. Autonomous robots that were once a topic of futuristic writing are heading for mass production today. Human...
-
APPLICATION
AI HARDWAREAPPLICATION -
ARTICLE
A 4-STEP GUIDE TO SELECTING PFC CONDUCTION MODE: CRM/DCM VS. CCMARTICLEThe power factor correction (PFC) boost converter is the industry-standard topology for meeting harmonic current regulations such as IEC 61000-3-2. This circuit is essential in modern AC/DC power supplies, where it shapes the input current (IIN) to follow the input voltage (VIN) sinusoidal waveform, achieving a power factor near unity. The key to successful PFC design lies in its operating mode. ...
-
ARTICLE
UNDERSTANDING ACCURACY AND RESOLUTION FOR MAGNETIC ANGLE SENSORSARTICLEMagnetic position sensors, especially magnetic angle sensors, are the fundamental building blocks of countless motion-control applications that necessitate precision positioning. These sensors are pivotal in a wide range of industries, from automotive and robotics to consumer electronics and medical devices, underscoring their universal appeal and importance (see Figure 1). However, to ...
-
ARTICLE
FILTERING HIGH-FREQUENCY INTERFERENCE IN STEP-DOWN CONVERTER DESIGNS WITH HOT-LOOP COMPONENTSARTICLEModern step-down converters are becoming increasingly efficient. In the frequency range of several hundred MHz, step-down converters can emit higher levels of interference. New IC designs and clever layouts are already able to compensate for such disturbances. By implementing high-frequency ferrite beads, interferences can be further effectively eliminated. In this article, an automotive expert d...
-
REFERENCE DESIGN
TITANIUM TI135REFERENCE DESIGNBoard Description: The Ti135 FPGA features the high-density, low-power Efinix® Quantum® compute fabric wrapped with an I/O interface. MPS solutions help optimize real-time edge applications where size, thermal efficiency, and power matter most. Ti135 M.2 Applications: Industrial cameras, roboti...
-
ARTICLE
THE POWER OF DUAL-PHASE DRMOS TECHNOLOGY IN AI SYSTEMSARTICLEAs AI systems continue to push boundaries, current demands are rapidly increasing. Next-generation AI systems face a critical layout bottleneck caused by escalating current demands that now frequently reach the 1000A to 2000A threshold per socket. To supply this immense demand for low-voltage power stably while minimizing ripple, voltage regulator module (VRM) architectures are forced to aggressi...
-
APPLICATION NOTE
AN245 - CALIBRATION OF THE MA600AAPPLICATION NOTEThe MA600A sensor integrates a 32-point lookup table designed for in-system calibration. This table stores correction values that are added to the measured angle to compensate for measurement inaccuracies. To determine the appropriate correction for any angle, the sensor performs linear interpolation between the two nearest calibration points. Calibration serves to mitigate errors arising from mag...
-
REFERENCE DESIGN
IND881REFERENCE DESIGNiND881 Evaluation kit
-
REFERENCE DESIGN
IND880REFERENCE DESIGNiND880 Evaluation kit
Log in to your account
Create New Account