Understanding the Role of a Battery Management System (BMS) in Electric Vehicles

DOWNLOAD PDF

Get valuable resources straight to your inbox - sent out once per month

Subscribe

We value your privacy

Electric vehicles (EVs) have become a ray of hope as the globe strives to address the issues of climate change and environmental sustainability. These electric-only vehicles mark a huge advancement in our search for greener, more environmentally friendly transportation options. The battery — a crucial element that determines the performance, safety, and efficiency of the EV — is at the core of these cars. The battery management system (BMS) is a sophisticated piece of technology that performs the complicated operation of managing this battery.

What is a Battery Management Systems (BMS)?

The battery management system is an electronic system that controls and protects a rechargeable battery to guarantee its best performance, longevity, and safety. The BMS tracks the battery’s condition, generates secondary data, and generates critical information reports. The state of charge (SOC), state of health (SOH), and residual capacity are three important metrics tracked and calculated by the BMS. Additionally, it monitors crucial variables like current, voltage, and temperature. Furthermore, the BMS actively guards the battery against risks like deep discharge, overcharging, overheating, and over-current conditions.

In addition to providing protection, the BMS regulates the environment of the battery by controlling the heating or cooling systems to keep the battery working within its ideal temperature range. Cell balancing is another crucial BMS function is that it ensure that each cell in a battery pack charges and discharges uniformly, enhancing the battery's overall performance and durability. Modern rechargeable batteries’ dependability and safety are maintained by this system’s extensive monitoring, reporting, and protection functions.

The BMS functions as the battery pack’s “brain” in several ways. It makes judgments depending on the information it gathers, and these choices have an impact on the battery's performance and longevity. Without a BMS, a battery might be overcharged or over-discharged, both of which have the potential to shorten its lifespan and cause battery failure.

The Role of the BMS in Electric Vehicles

The BMS is typically an embedded system and a specially designed electronic regulator that monitors and controls various battery parameters (e.g. temperature, voltage, and current) to keep the battery cells within a safe working range. Figure 1 depicts the overall structure of a BMS used in electric vehicles. The input, data processing, and output signals used in the BMS can be used to depict the data flow according to the architectural design.

Figure 1: Internal architecture of BMS in an electric vehicle

The BMS serves a number of critical functions in the context of electric vehicles, including monitoring, protection, balancing, and thermal management. These functions are described in greater detail below.

Monitoring

The battery’s voltage, current, temperature, and SOC are all constantly monitored by the BMS. To evaluate the battery's performance and condition, this information is essential. As an example, the SOC, which measures the battery’s remaining charge, has a direct impact on the EV's driving range.

The BMS also keeps track of the battery’s SOH, which is a gauge of its general health. The SOH can give early warnings of prospective battery issues, enabling preemptive maintenance or enabling the replacement of faulty cells.

Protection

The BMS protects against probable problems that can hurt the battery and, consequently, the car. These protections include over-current (OC), over-voltage (OV), under-voltage (UV), over-temperature (OT), and under-temperature (UT) conditions. The BMS guarantees the battery’s longevity and safety by prohibiting it from running outside of its safe operating area (SOA).

Over-current protection (OCP) safeguards the battery against high currents that exceed the battery’s permitted current rating and could lead to overheating and battery damage. In order to prevent the battery from being charged or discharged beyond what is safe, which could otherwise result in a shorter battery life or even battery failure, over-voltage protection (OVP) and under-voltage protection (UVP) are used. The battery functions within a safe temperature range thanks to over-temperature protection (OTP) and under-temperature protection, which prevent harm from extreme heat or cold.

Balancing

Another crucial job of the BMS is battery balancing. It’s critical to maintain an even charge across all cells because an EV battery pack is made up of numerous individual cells. The BMS does this via active or passive balancing, enhancing the battery pack's general effectiveness and durability.

During active balancing, the charge is moved from higher-charged cells to lower-charged ones to maintain the same charge level in all the cells. On the other hand, the use of shunt resistors in passive balancing causes the excess charge from higher-charged cells to be dissipated as heat, instead of being transferred between cells. By charging continuously without dissipating, the lower-charged cells can catch up using this technique. Over several charge cycles, passive balancing gradually improves the state of charge uniformity across the cells by preventing any one cell from being overcharged. Both techniques attempt to increase the battery pack's capacity and lifespan, but active balancing is more effective because it redistributes the charge rather than dissipating it as heat.

Thermal Management

The BMS is essential for controlling the temperature inside the battery pack. It assists in preventing overheating, a scenario that could result in shortened battery life or even thermal runaway, by monitoring the temperature and deploying cooling techniques as needed.

A dangerous situation known as a thermal runaway occurs when a spike in temperature causes further increases in temperature, which could result in an uncontrollable, destructive response. The BMS can stop thermal runaway and guarantee the battery's safe operation by monitoring the temperature of the battery cells and acting as needed.

The Future of BMS in Electric Vehicles

Battery management systems (BMS) are becoming increasingly complex as EV technology develops. It is expected that the future BMS will include cutting-edge capabilities like predictive analytics for greater performance optimization, increased safety protocols, and improved integration with other vehicle systems.

Using historical data and machine learning algorithms, predictive analytics make predictions about the future. This can entail projecting past performance to forecast the battery’s future state-of-charge (SOC) or overall health, in the context of a BMS. This would make it possible to manage the battery more proactively, thereby extending its lifespan and enhancing the efficiency of the EV.

Improved safety standards might include more sophisticated techniques for anticipating and avoiding potential battery issues. This might require more complex algorithms for spotting irregularities that might point to a possible issue as well as more comprehensive monitoring of the battery's condition.

The BMS could communicate more directly with other EV systems, such as the motor controller or the onboard computer, to improve integration with other vehicle systems. This may make it possible for the car to operate more smoothly, which will enhance its effectiveness, performance, and user experience.

Conclusion

In summary, the battery management system (BMS) is a crucial part of electric vehicles that manages, safeguards, and monitors the battery. Understanding the nature and purpose of the BMS will help us better appreciate the intricate technological interplay that powers both current and future electric vehicles.

The BMS will certainly move forward and change as we continue to advance and stretch the limits of what is feasible with electric vehicles. We can make sure we are utilizing the potential of this technology to create safer, more effective, and more sustainable electric vehicles by keeping up with these improvements.

Understanding the function and significance of the BMS is essential whether you work for an electric vehicle manufacturer, create BMS systems, or are just a fan of the technology. The BMS will continue to be a key component of this innovative field of technology as we approach a future where electric cars are widely used.

_______________________

Did you find this interesting? Get valuable resources straight to your inbox - sent out once per month!

Get technical support