Scalable Current-Sharing E-Fuse Solution
by Jason Bone
DOWNLOAD PDFIn typical hot-swap or electronic fuse (e-fuse) applications, great care must be taken when selecting the MOSFET to ensure that the safe operating area (SOA) of the device is not exceeded during a soft-start (SS) turn-on. Even if multiple MOSFETs are paralleled, the soft-start condition causes large amounts of thermal stress.
Generally, when using discrete MOSFETs in hot-swap and e-fuse applications, it is assumed that only one MOSFET is conducting the entire soft-start current. This is due to the variation in the gate threshold voltage of each MOSFET. Therefore, all the power loss is in one device even though there may be multiple MOSFETs in parallel. This requires oversizing the MOSFET rating and package size, which drives up the PCB area. With typical hot-swap/e-fuse applications, a precision current sense resistor and a controller is needed to provide SS timing, temperature protection, and over-current protection (OCP).
The MPS MP5921 provides an innovative hot-swap/e-fuse application with a simple and stackable building block. The MP5921 has a built-in MOSFET, current sensing, temperature sensing, soft-start ramp control, and advanced protection features. The use of advanced monolithic processes allows for user-friendly implementation for hot-swap and e-fuse solutions (Figure 1)
Figure. 1: Hot-Swap/E-Fuse Application Components
The MP5921 uses an advanced monolithic process to monitor and drive the internal MOSFET actively during the soft-start process to ensure the SOA of the MOSFET. Using this monolithic process, the MP5921 can measure the current flowing through the internal MOSFET accurately.
With the ability to monitor the current through the internal MOSFET, multiple MP5921 devices connected in parallel actively balance the current flowing through each device during the soft-start condition. This ensures that each device carries the soft-start current equally and that no one device carries the full soft-start load current. With the soft-start current balanced among the devices in parallel equally, the risk of violating the SOA of the MOSFET is reduced greatly, and the thermal energy is more evenly distributed on the PCB.
Figure 2 shows the current sharing of three MP5921 devices in parallel during a soft start with a DC load. All three devices in parallel share the soft-start load current evenly.
Figure 2: Three MP5921 Devices in Parallel
If the traces for the individual currents are set on the same origin point, it can be seen that they overlap exactly (Figure 3)
Figure 3: Currents with Same Origin Point
The MP5921 can be scaled to support any current range needed for hot-swap and e-fuse solutions. With a 60-A current rating in a 4 x 5-mm package, the MP5921 provides an extremely dense hot-swap/e-fuse solution. Each MP5921 has built-in protection features that monitor damaged MOSFETs, over-temperature conditions of the internal MOSFET, soft-start watchdog timer, and over-current protection.
The MP5921 also has a built-in short-circuit protection (SCP) feature that can disable the internal MOSFET within 200 ns of a short detection. This quick disabling function prevents a large buildup of current on the PCB where output shorts occur.
The MP5921 provides a robust and user-friendly solution for space-critical designs that can be scaled to meet the design requirements of all types of hot-swap/e-fuse applications.
______________________________
Did you find this interesting? Get valuable resources straight to your inbox - send out once per month!
Technical Forum
Latest activity 5 days ago
4 Comments
Latest activity 6 days ago
5 Comments
Latest activity 6 days ago
1 Comment
Log in to your account
Create New Account