Understanding Quiescent Current and Shutdown Current with a Boost Converter
DOWNLOAD PDF
Get valuable resources straight to your inbox - sent out once per month
We value your privacy
Introduction
For battery-powered applications, an excellent user experience depends on a long battery life and high-performance terminal devices. Quiescent current (IQ) is an important parameter to consider when optimizing these applications; in particular, an improved IQ increases battery life.
This article will describe the difference between a boost converter’s IQ and shutdown current (ISD) to provide a deeper understanding of how IQ and ISD can be utilized in battery-powered applications.
Battery Types
In many battery-powered applications, the battery output is relatively low, such as a 1.5V output voltage (VOUT) from a single AA battery. Meanwhile, the back-end IC or subsidiary circuit requires a higher input voltage (VIN). In these systems, a step-up converter (also known as a boost converter) is typically used to step up the voltage from a battery output. Otherwise there is an insufficient VIN for the IC or subsidiary circuit.
Figure 1 shows a few different battery types, such as cylindrical batteries, coin batteries, and phone/tablet batteries.
Figure 1: Battery Types
Table 1 shows battery types and their typical output voltages.
Table 1: Battery Types and their Typical VOUT
| Type/Spec | Cylindrical Batteries | Coin Batteries | Phone/Tablet Batteries | |||||
| NiMH | Lithium-Iron | Lithium-Ion | NiCd | CR | SR | LR | Lithium-Ion | |
| VOUT | 1.2V | 1.5V | 3.7V | 1.2V | 3V | 1.55V | 1.5V | 3.7V |
| Sizes | A, AA, AAA, AAAA, C, D, N, and F | Varies | ||||||
Batteries should be selected based on the application needs. However, note that the maximum VOUT among these batteries is 3.7V, which may be insufficient for a number of applications. This is when a boost converter becomes vital.
Related Content
-
WEBINAR
MPS On-Board Charging Solutions
Power electronics have become paramount in the design of on-board chargers, traction inverters, and DC/DC converters
-
ARTICLE
Voltage Regulator Types and Working Principles
MPS offers a variety of efficient, compact linear and switching voltage regulators, including the HF500-x family, MP171x family, MP20056, MP28310, MPQ4572-AEC1, and MPQ2013-AEC1
-
REFERENCE DESIGN
MPQ3426 - Pre-Boost Reference Design, Simple Solution to Cold-Crank Transients
This reference design will help engineers designing a pre-boost for a power supply up to 18W
-
ARTICLE
High Power, Fully Integrated, Synchronous Boost Converter with Optimized Features for Portable and Battery-Operated Applications
The MP3432 from MPS is a perfect choice for the first stage of battery-powered systems
Boost Converters
MPS provides a variety of synchronous step-up (boost) converters that can be used to step up a battery’s VOUT such that it can provide a sufficient VIN for the receiving system. The remainder of this article will focus on the differences between a boost converter’s ISD and IQ while using the MP28600, an ultra-low IQ, synchronous boost converter. The MP28600 is a brand new IC solution with nA level quiescent current and a small SOT563 (1.6mmx1.6mm) package. It is well-suited for wearable devices, industrial sensors, and battery-powered, handheld medical instruments.
Shutdown Current (ISD)
ISD is the current drawn by the IC from a battery when the IC is switched off and the battery is still connected to the system. Consider the scenario in which the MP28600’s enable signal is set to 0V, and it is connected to a battery with a VIN that is equal to 3.3V. ISD is the current measured from the input (see Figure 2).
Figure 2: Measuring ISD
It may be difficult to understand why the IC consumes current even though it has shut down. This is because some of the internal circuitry, such as the start-up loop, still leak small amounts of power to the ground (GND); this leakage consumes battery current (see Figure 3).
Figure 3: ISD in an IC Circuit
Consider the following real-world example. If you buy a battery-charged electrical device from the store, and that device has been on the shelf for a significantly long time, then you may not be able to turn it on until it has been sufficiently charged. This is because the IC continuously consumes a certain ampere of current from the battery. In addition, when the battery is over-discharged, it can be damaged and have a reduced full-charge capacity if there is no protection.
Quiescent Current (IQ)
IQ is the current consumed by the IC when it is enabled (but not switching), or when there is no load applied. This current can also be called operating quiescent current, standby current, and sleep mode current.
For example, set the MP28600’s enable signal to 5V. The IC is connected to the battery, which has a VIN of 3.3V. IQ is the measured current from the MP28600’s input voltage pin (see Figure 4).
Figure 4: Measuring IQ
Similar to ISD, it may be difficult to understand why there is an IQ. Even if there is no load and the IC is not switching most of the time, some of the internal circuitry continues operating to maintain the device’s basic functions, which requires a small amount of current. Figure 5 shows a control loop that consumes current.
Figure 5: IQ in an IC Circuit
Consider the following real-world example using a security sensor (see Figure 6). IQ is essential for applications that run in a sleep state. 99% of the time, a security sensor does not detect an object or hazardous condition that triggers the alarm; however, it cannot shut down. In this scenario, the sensor can operate in sleep mode and wake up only when necessary. While in sleep mode, the IC consumes a small amount of power from the battery — this current is the operating IQ. The smaller the IQ, the longer the battery life.
Figure 6: Security Sensor Functionality
Conclusion
This article used the MP28600, a step-up (boost) converter, to describe the differences between quiescent current and shutdown current, which can be optimized in battery-powered applications. As electrical devices become more intelligent and diverse with evolution of Internet-of-Things (IoT) devices, portable applications, medical instruments, and industrial sensors, low power consumption and a small size are paramount.
MPS provides a robust portfolio of converters to meet any application’s needs.
_______________________
Did you find this interesting? Get valuable resources straight to your inbox - sent out once per month!
Log in to your account
Create New Account