Understanding Frequency Spread Spectrum: The Benefits and Limitations of Using FSS in Modern SMPS Designs
Get valuable resources straight to your inbox - sent out once per month
We value your privacy
Abstract
Modern passenger vehicles are not only made to carry passengers from one destination to the next — they must also function as communication tools, TVs, home cinema sets, LED illumination centers, and even massage parlors. The customer’s focus is changing from purely driving characteristics (e.g. horsepower and acceleration) to include entertainment systems, such as the size of the multimedia touchscreens and the ability to access mobile networks.
The vehicle of tomorrow must be able to connect to social media, stream UHD videos, and keep passengers online, as well as communicate with other vehicles, infrastructure, and pedestrians to enable autonomous driving. On top of that, these cars must maintain older features such as classic electrical control units (ECUs) for features like radio tuners and GPS navigation. This leads to a rising number of ECUs.
The rise of vehicle electrification requires solutions with efficient and powerful power conversion. These solutions are expected to have small form factors for power supplies. Having excellent efficiency and a small form factor requires high switching frequencies as well as very fast switching flanks on the switching point of the switch-mode power supply (SMPS), which poses challenges for EMC engineers.
This article will explore how frequency spread spectrum (FSS) can be used to effectively reduce the EMI spectrum of a power supply in specific frequency bands, as well as related physical limitations.
Understanding Frequency Spread Spectrum (FSS)
To understand how FSS works, let’s look at the spectrum of a traditional SMPS such as the MPQ4371-AEC1. The MPQ4371-AEC1 is an automotive buck regulator that can achieve up to 11A of continuous output current (IOUT) with zero-delay PWM (ZDPTM) control and a switching frequency (fSW) up to 2.5MHz.
Figure 1 shows the spectrum of this SMPS when the main fSW is set to 2.2MHz. The corresponding harmonics can be calculated as (n x fSW), where n is the corresponding harmonic.
Figure 1: Spectrum of a Traditional SMPS
The power of the harmonics decreases with higher measurement frequencies, and it disappears in the noise floor at about 400MHz. Each peak in the spectrum (calculated with n x fSW) is shown with the resolution bandwidth (RBW) and the filter type used by the spectrum analyzer.
The RBW filter is defined by the minimum and maximum frequency, as well as the filter order. RBW determines the settling time (tS) for the RBW filter, calculated with Equation (1):
$$t_s=\frac{1}{RBW}$$Figure 2 shows a traditional RBW filter of a spectrum or signal analyzer.
Figure 2: RBW Filter Characteristics
By measuring a spectrum, the spectrum analyzer sweeps through the defined frequency area. Whenever there is a peak inside the RBW filter, this specific frequency is shown in the scope (see Figure 3). This provides the possibility to move power from each specific harmonic inside the area between the peaks.
Figure 3: Resolution Bandwidth Filter and Switching Frequency in the Spectral Area
Figure 3 shows that a higher RBW combined with a smaller fSW will move the spectrum closer together. This means the energy of the harmonics can only be transferred to a smaller area. Theoretically, if all the energy of the peaks is transferred into white noise, the attenuation (α) of each specific peak is linked to fSW and RBW, estimated with Equation (2):
$$α=10 x log (\frac{RBW}{f_{SW}})$$Figure 4 shows the relationship between the maximum theoretical attenuation, which can be achieved via FSS, alongside the corresponding RBW and fSW. As an example, assume that the SMPS’s fSW is 0.5MHz, and the RBW is 120kHz; the maximum attenuation that can be achieved with FSS is 6.2dB.
Figure 4: Maximum Possible Theoretical Attenuation for FSS
Transforming a Specific Spectrum to Frequency Spread Spectrum (FSS)
To transform the SMPS’s original spectrum to FSS, we must dither around the original switching frequency.
Figure 5: Modulation Signal for FSS Showing the Context of fSPAN and fMOD
To dither around the original switching frequency, consider the following:
- tS: The RBW’s settling time must be considered. If the time for the frequency to change (the modulation frequency, or fMOD) is longer than tS, there is no achievable attenuation with FSS.
- RBW: Because if the dither frequency (fSPAN) is smaller than the RBW, the frequency dithers within the filter’s bandwidth, and the attenuation with FSS is zero.
When considering the two rules above, it can be concluded that fSPAN must exceed the RBW, calculated with Equation (3):
$$f_{SPAN}>RBW$$Meanwhile, fMOD must exceed the inverse of tS, estimated with Equation (4):
$$f_{MOD}>\frac {1}{t_s}, \text{with} t_s=\frac{1}{RBW}$$The frequency change (fSPAN x fMOD) can be calculated with Equation (5):
$$\text{Frequency Change}=f_{SPAN} \times f_{MOD} > RBW^2 [\frac{Hz}{s}]$$Table 1 shows the frequency change values to achieve FSS within specific RBWs.
Table 1: Frequency Changes to Achieve Attenuation
| RBW | Settling Time | Minimum Frequency Change |
| 9kHz | 111µs | 81MHz/s |
| 120kHz | 8.33µs | 14.4GHz/s |
| 1000kHz | 1µs | 1THz/s |
To generate a white noise signal and be compliant with the two rules above, we need to dither from zero to infinity within a period very close to zero. As this is technically impossible, the dither frequency (fSPAN) should be between 10% and 20% of the original fSW. This will provide enough fSPAN to ensure a good attenuation, and it will keep the SMPS at a stable operating point.
Real measurements show that the attenuation with FSS is most effective when the modulation frequency (fMOD) is almost equal to the spectrum analyzer’s RBW.
For example, consider a scenario where fSW is 2MHz and fSPAN is 20%. Table 2 shows fMOD and the frequency change for this scenario.
Table 2: Frequency Change for Given Working Areas
| Modulation Frequency (fMOD) | Header |
| 9kHz | 3.6GHz/s |
| 120kHz | 48GHz/s |
By comparing Table 1 and 2, it can be observed that it is possible to achieve great attenuation for an RWB of 9kHz with an fMOD of 9kHz. However, the attenuation with an RBW of 120kHz is 0 since the frequency change is too slow. To achieve reasonable attenuation for a 120kHz RBW, we must increase the FSS frequency.
Because FSS is always modulated to the SMPS’s switching frequency, high harmonics will automatically reach a high frequency change at their dedicated frequency (see Table 3).
Table 3: Corresponding Frequency Change for the SMPS’s Harmonics
| Harmonic | Spectral Frequency | fMOD | fSPAN (20%) | Frequency Change |
| fSW | 2MHz | 9KHz | 400kHz | 3.6GHz/s |
| Second harmonic | 4MHz | 9KHz | 800kHz | 7.2GHz/s |
| Third harmonic | 6MHz | 9KHz | 1200kHz | 10.8GHz/s |
| Fourth harmonic | 8MHz | 9KHz | 1600kHz | 14.4GHz/s |
Modulation Waveforms
After establishing the correlation between fMOD and fSPAN, we can consider the modulation waveform. Because the frequency change during normal operation should be linear, the easiest way to modulate FSS is by using a triangular modulation signal (see Figure 5). This is simple to implement, but at the signal’s edges, the frequency change within a specific timeframe is half of the frequency change during the rising or falling flank (f / 2).
To prevent this, it is possible to use a sawtooth waveform, where the frequency change is linear while ramping. After receiving the maximum fSW, the SMPS changes from the maximum to minimum fSW within one switching cycle. However, this can cause control loop instability and output voltage (VOUT) undershoot or overshoot.
Therefore, mixing different waveforms (e.g. the “Hershey’s Kiss” waveform or a stepped triangular waveform) are ways to optimize attenuation while maintaining SMPS stability.
Figure 5 shows the different FSS modulation waveforms.
Figure 6: Different FSS Modulation Waveforms
All of these waveforms have one thing in common: They can only be used with one specific modulation frequency (fMOD).
From the rules in the paragraph above, fMOD should be within the frequency area of the RBW to achieve the best possible attenuation. When checking the CISPR 25 norm, there are two very critical frequency areas for SMPS developers:
- The rod-antenna measurement, which goes from 150kHz to 30MHz with an RBW of 9kHz.
- The biconical-antenna measurement, which goes from 30MHz to 300MHz and has its toughest limits with an RBW of 120kHz.
As these two measurements use two different RBWs, the FSS fMOD can only be optimized for one specific frequency area.
To optimize FSS for the full spectrum, the MPQ4371-AEC1 offers dual-FSS modulation (see Figure 7).
Figure 7: MPQ4371-AEC1 Dual-FSS Modulation Waveform
Using this modulation waveform provides the benefits of FSS within the low-frequency (LF) and high-frequency (HF) spectrum. The main carrier (fMOD(LF)) has a frequency of 15kHz, which is optimized to achieve an attenuation on the SMPS spectrum with the rod-antenna measurement. Ideally, fMOD(LF) should have a frequency of 9kHz, but this frequency can cause audible noise from the SMPS. To avoid this, fMOD(LF) can be increased to 15kHz. This gives nearly the same attenuation as the 9kHz modulation frequency and avoids audible noise. The second frequency is modulated on the carrier frequency with 120kHz, which provides an additional attenuation for the biconical antenna measurement. Using dual-FSS modulation provides the possibility to tune the specific modulation frequency’s fSPAN for each given use case. The MPQ4371-AEC1 provides eight different FSS options to allow for further fine-tuning (see Table 4).
Table 4: FSS Options for the MPQ4371-AEC1
| fSPAN Options | fMOD(LF) (15kHz) | fMOD(HF) (120kHz) |
| fSPAN 1 | - | - |
| fSPAN 2 | 10% | - |
| fSPAN 3 | 6.2% | - |
| fSPAN 4 | 8.6% | 2.5% |
| fSPAN 5 | 6.2% | 2.5% |
| fSPAN 6 | 6.2% | 4.3% |
| fSPAN 7 | 4.8% | 2.5% |
| fSPAN 8 | 4.8% | 4.3% |
Practical Measurements
To show the effects of the different types of FSS, we can compare different versions of the MPQ4371-AEC1 on a real evaluation board with identical settings. The standard evaluation board for the MPQ4371-AEC1 (1) was used in a CISPR 25 EMC chamber, and the measured frequency range was between 150kHz and 1GHz. To compare the effects of FSS, three modes were tested:
- The MPQ4371-AEC1 without FSS (green trace)
- The MPQ4371-AEC1 with 15kHz FSS and a ±10% span (blue trace)
- The MPQ4371-AEC1 with dual-FSS: 15kHz FSS and a ±6.2% span, and 120kHz FSS with a ±2.5% span (yellow trace)
Note:
1) Contact an MPS FAE for details on this evaluation board.
In all three scenarios, the MPQ4371 ran with a 2.2MHz fSW and a 3A load. Figure 8 shows the measurements captured via the rod-antenna method with an RBW of 9kHz.
Figure 8: EMC Measurements for Three Different Types of FSS (Rod-Antenna)
Figure 9 shows the EMC spectrum in the frequency area between 30MHz and 1GHz with a RBW of 120kHz.
Figure 9: EMC Measurements for Three Different Types of FSS (Biconical and Log-Periodic Antenna)
Figure 8 and Figure 9 show that FSS can make a huge difference on the SMPS’s frequency spectrum. Especially for the rod-antenna measurement, FSS can effectively reduce the peaks at the fundamental switching frequency and the first harmonics. In this scenario, a maximum attenuation of 14dB is achieved.
For the rod-antenna measurement, the single 15kHz FSS is more effective than the dual-FSS method, since the frequency span is bigger for that modulation (10% with single-FSS vs. 6.2% with dual-FSS).
However, higher frequencies benefit from the dual-FSS method, especially in the 40MHz to 140MHz range. Dual-FSS provides an additional benefit of up to 3dB since fMOD stays within the RBW.
Conclusion
Frequency spread spectrum is an effective method to provide attenuation to the spectrum of an SMPS. Care must be taken regarding the modulation frequency and the frequency span, as these are two critical limitations that can result in no attenuation at all. In addition, the modulation waveform plays a role, since using single-FSS or dual-FSS influences different frequency areas, whereas each specific waveform (e.g. triangular or sawtooth) also influences the stability of the SMPS.
Ultimately, using FSS should be a case-by-case decision. FSS should be tuned such that the most sensitive frequency areas provide the most attenuation within the SMPS spectrum, which makes devices such as the MPQ4371-AEC1 ideal, as it provides up to 8 different FSS options. Visit the MPS website to find an automotive-grade step-down converter that can meet you design needs.
_______________________
Did you find this interesting? Get valuable resources straight to your inbox - sent out once per month!
Log in to your account
Create New Account