Portable Media Players
Portable Media Players Content
Description
Our comprehensive portfolio of solutions includes switches, drivers, converters,chargers, and amplifiers. Each part is designed for the best efficiency in the smallest package size. Our expertise and innovation mean that each solution offers exceptional signal-to-noise and power supply rejection ratios, and helps simplify system design.
MPS provides efficient, cost-effective solutions across the signal chain for next-generation portable media player designs.
Block Diagram
Select parts to expand information in chart below
Components List
Resources
-
UNDERSTANDING QUIESCENT CURRENT AND SHUTDOWN CURRENT WITH A BOOST CONVERTERFor battery-powered applications, an excellent user experience depends on a long battery life and high-performance terminal devices. Quiescent current (IQ) is an important parameter to consider when optimizing these applications; in particular, an improved IQ increases battery life. This article will describe the difference between a boost converter’s IQ and shutdown current (ISD) to provide a de...
-
ARTIX ULTRASCALE+ AU10P/15P MINIMUM RAILS – HIGHEST POWER REFERENCE DESIGN -
ARTIX ULTRASCALE+ AU10P/15P MINIMUM RAILS – SMALLEST SIZE -
ZYNQ ULTRASCALE+ MPSOC 7 RAIL DISCRETE POWER MANAGEMENT REFERENCE DESIGNThis is a scalable design for powering the AMD Xilinx Zynq UltraScale+ MPSoC family (ZU2 to ZU19). This discrete solution combines a small footprint with excellent efficiency and tight regulation. An external sequencer meets power up and power down sequencing requirements.
-
IOTMPS works closely with Qualcomm to create power solutions for their IoT products supporting 802.11a/b/g and 802.15.4 standards The MPS components on these reference designs are carefully selected to meet price and performance objectives of these designs. Please contact your regional MPS contact or use the displayed link below for assistance
-
WIFIMPS works closely with Qualcomm to create power solutions for all their WiFi products supporting 802.11ax including WiFi6 standards with 2.4GHz/5GHz/6GHz bands The MPS components on these reference designs are carefully selected to meet price and performance objectives of these designs. Please contact your regional MPS contact or use the displayed link below for assistance
-
VERSAL ACAP HIGHEST EFFICIENCY 8 POWER RAIL REFERENCE DESIGNEVREF0105A
-
HIGH POWER, FULLY INTEGRATED, SYNCHRONOUS BOOST CONVERTER WITH OPTIMIZED FEATURES FOR PORTABLE AND BATTERY-OPERATED APPLICATIONSBy Jing “Mirror” Yang, Senior Product Marketing Engineer, and Panyin Liu, Manager, Systems and Applications Engineering, Monolithic Power Systems The superior properties of Li-ion batteries, such as high energy density, light weight, no memory effect, and less self-discharge, make them a very popular option in portable applications. ICs with boost topology are needed in portable...
-
DC FAST CHARGING STATIONDC fast charging stations are becoming more common with the increased adoption of electric vehicles. Charging stations are a vital part of the infrastructure along major highways and populated suburbs, ensuring that electric vehicles have a place to charge during long-distance travel and day-to-day driving. These systems are often comprised of multiple 25kW to 75kW modules to create fast charging ...
-
MPS POWER MANAGEMENT SOLUTIONS FOR POWER OVER ETHERNET (POE) SWITCHESModern devices are increasingly powered by Power over Ethernet (PoE), such as IP phones, wireless APs, and IP cameras. Customer premise equipment (CPE) and small base stations in the 5G era also require PoE power. Figure 1 shows common applications powered by PoE. This article discusses MPS’s comprehensive suite of power management solutions for a wide range of switches, including PSE, boo...
-
PROGRAMMABLE LOGIC CONTROLLER (PLC) -
LOAD-LINE DESIGN FOR A MULTI-PHASE BUCK CONVERTERWith the increase in 5G networks, cloud computing, Internet-of-Things (IoTs), and virtualization, IT infrastructure is driving the demand for high-performance computing servers. Each new server generation requires higher computing power and efficiency, while also increasing power requirements. One of the key aspects in ensuring that servers meet market demands is to understand the effect that the...
-
BATTERY CHARGER FUNDAMENTALSLi-ion battery charger ICs are devices that regulate battery charging current and voltage, and are commonly used for portable devices, such as cellphones, laptops, and tablets. Compared to other battery chemistries, Li-ion batteries have one of the highest energy densities, provide a higher voltage per cell, can tolerate higher currents, and do not have to be trickle charged when the battery is fu...
-
VERSAL PREMIUM - FULL MANAGEMENT (OPTIMIZED FOR EFFICIENCY) REFERENCE DESIGN -
VU57P ULTRASCALE+ EXTENDED PORTFOLIO HIGHEST SIZE POWER MANAGEMENT REFERENCE DESIGN -
E-TRACKER REFERENCE DESIGNTracking the location of different types of vehicles is an increasingly popular application for multiple purposes, such as control of transport trucks or anti-theft security. However, this presents two challenges in electronic design. First, the system must be able to track a vehicle’s location when the car battery is turned off. Second, the GSM modules that establish communication with the ...
-
ANALOG SIGNAL VS. DIGITAL SIGNALSA signal is an electromagnetic or electrical current that carries data from one system or network to another. In electronics, a signal is often a time-varying voltage that is also an electromagnetic wave carrying information, though it can take on other forms, such as current. There are two main types of signals used in electronics: analog and digital signals. This article discusses the correspond...
-
ZYNQ ULTRASCALE+ MPSOC 8 RAIL DISCRETE POWER MANAGEMENT REFERENCE DESIGNThis is a scalable design for powering the AMD Xilinx Zynq UltraScale+ MPSoC family (ZU2 to ZU19). This discrete solution combines a small footprint with excellent efficiency and tight regulation. An external sequencer meets power up and power down sequencing requirements.
-
SMART TRACKERSSmart trackers are one of the latest innovations in the growing market of wearable and highly portable devices. Intended to help the user track or find items such as keys, critical features include multi-standard wireless connectivity — such as Bluetooth, Wi-Fi, GPS, and near field communication (NFC) — as well as reliable sensing and feedback to communicate the devices location. These high levels...
-
GAMING CONTROLLERS & PERIPHERALSGaming controllers and peripherals are expected to have fast, accurate controls, reliable haptic feedback, and a long battery life. The nature of these devices means they must also be lightweight, comfortable to hold, and fairly durable. Connectivity options include RF signals, WiFi, Bluetooth, and near field control (NFC), and many controllers and peripherals integrate more than one of these. Oth...
-
ELECTRONIC SMART LOCKSElectronic smart locks are increasing in popularity with the rise of IoT and smart homes, as they provide convenience and a sense of security to consumers. Because they are typically battery-powered, energy efficiency to maximize battery life is crucial. The nature of these devices means they must also offer ease-of-use, stable operation, and the ability to withstand wide temperature ranges and ex...
-
AIR PURIFIERS & HUMIDIFIERSAir purifiers and humidifiers must be able to reliably improve air quality for end users. The best designs also offer improved energy efficiency, convenience, and low noise. As more and more appliances are expected to be smart-home ready, consumers are demanding new features such as wireless connectivity for ease of control. To meet and exceed customer expectations, designers are challenged with f...
-
MOBILE POSMobile points of service (POS) offer the same features as other portable POS devices from the convenience of a tablet or smartphone. POS are expected to deliver fast, secure payment transactions amid changing payment methods and rising customer expectations. They must offer high reliability, long battery life, ease-of-use, and quick processing speeds to accelerate checkout times. As retail and ser...
-
DRONE REMOTE CONTROLLERSDrone remote controllers must be able to offer consumers the precise, reliable control of drones and multicopters without hindering speed, navigation, or flight time. Wireless connectivity, as well as fast data processing and communication across a broad transmission distance, are crucial to ensure proper control and safety. Many new designs also feature LCD or LED interfaces, or even smartphone c...
-
IR CONTACTLESS THERMOMETERSHandheld thermometers provide a direct method for measuring personal body temperature. Contactless thermometers are crucial for cases in which measurements must be taken while minimizing the spread of viral and bacteria contaminants. This allows users in clinical settings, as well as homes and businesses, to get instant results while minimizing contaminant propagation. These portable devices requi...
Log in to your account
Create New Account