行业信息

行业信息

项目主题发行日期
新闻中心

发送最新文章至您的收件箱

文章:喜报!MP2888A产品获得2018年全球电子成就奖——“年度电源管理器”

上周在全球电子技术领域最大媒体集团ASPENCORE主办的全球双峰会上揭晓了2018年全球电子成就奖名单,MPS公司的MP2888A作为业界首款10相数字控制器获得了“年度电源管理器”的称号。全球获得此奖项的只有三家公司,MPS就是其中一家。

原文发表在 WeChat.

2018.12
文章: Energy Recycling in DC Motor Drives

When decelerating a moving mass in a permanent magnet motor drive, energy stored in the mechanical system may be returned through the motor driver to the power source. If this energy is not properly accounted for, it can cause damage to the motor driver or the rest of the system by causing an increase in the power supply voltage.

In this article, we will look at ways to dissipate this energy safely. To simplify the examples, a DC brush motor is shown. This applies to brushless motor systems as well.

原文发表在 EDN.

 2018.11
文章:The Linear Charger in Wearable Applications

Wearable devices have become increasingly integrated into our lives. In addition to being used in fitness devices, they have also worked their way into other fields, including medical care, entertainment, security, and finance. In all applications, battery life and component size are two key concerns. Most applications require a small board and low BOM, which means the device should be highly integrated. 

Our new article discusses common issues in earable device applications, including size, programmability, and battery life, and how these issues can be resolved with the MPS MP266x line of linear chargers.

原文发表在 Bodo's Power Systems (page 78).

2018.11
文章:大功率全集成同步 Boost 升压变换器,可优化便携式设备和电池供电应用

众所周知,锂离子电池能量密度高、重量轻、无记忆效应、自放电小,在便携式应用领域中备受青睐。但是,由于大多数锂离子电池的电压范围在 4.2V (完全充电) 至 3.0V (完全放电)之间,而后级电路的输入电压会高达 12V 或更高,因此在便携式应用中需要采用升压拓扑集成电路。市面上的便携式应用(例如蓝牙音箱、快充移动电源及便携式 POS 机),所常用的 Boost 升压产品有: 带外部 MOSFET 的控制器方案,带外部二极管的非同步 Boost 升压变换器方案,或者输入/输出范围有限的升压方案。但以上解决方案,存在诸多缺点:其占用空间大,组成部件多,效率也比较低,且在噪声和可靠性方面拉低了整体产品的性能。

原文发表在 Codico Impulse.

2018.10
网络研讨会:可通过网站编程的电源模块

MPS web programmable DC DC power modules allow for rapid prototyping and getting products to market faster. Learn how using web based software allows quick hardware changes. Our website configuration and simulation tool allows you to easily enter your load requirements, change your output voltage, adjust your passive component parameters and instantly evaluate your design performance. Changes to design can be made immediately, eliminating time consuming system verification and board rework, dramatically reducing design time.

Web Programmable DC DC Power Module Webinar

2018.10
文章:分析和仿真PCB 交流电阻损耗,优化DrMOS核心电压

作为开关电源损耗的一部分,印刷电路板(PCB)主回路纹波电流阻抗的损耗常被忽略不计。然而,对于采用大电流核心电压和高纹波电流工作的应用而言,这种损耗却不容忽视。使用Ansys Q3D,可以提取典型核心电压功率级 PCB 布局中主回路纹波电流的频变电阻参数,还可以看出这一损耗成分是如何显著改善建模与测量总损耗之间的相关性(开关频率函数)。为了在负频率系数PCB与无源元件损耗和正频率系数MOSFET常规开关损耗之间的平衡点处达到峰值效率,我们提出了一种优化开关频率的解析表达式。

原文发表在 EDN.

2018.9
文章:电容隔离: AC/DC功率转换产品未来基本组成部件

经历过去十年的发展,电容隔离俨然已经成为一种成熟的解决方案,常被用来取代使用在信号隔离器、隔离栅极驱动、隔离收发器等应用中的光耦合器1 。然而,电容隔离的另一种潜在应用却常常被忽视,即用来取代离线适配器中的光耦合器。本文将阐释,为什么电容隔离将成为未来AD/DC功率转换的基本构成部分,它又是如何在性能方面超越其他隔离技术的,以及它给终端应用带来的独特优势。

原文发表在 Power Systems Design.

2018.9
文章:即插即用型数字可编程电源模块实现了电源快速成型技术

在电子产品开发过程中,设计师常常会面临两种挑战:项目延迟和成本超支。产品规格变更和技术规格不达标成为项目延迟和预算超支的两个最常见原因。有时电源工程师不得不因规格变更而彻底推翻先前方案,重新设计。任何一个电子产品的开发,都逃不开电源设计。电源的设计优劣,轻则影响整个产品的性能,重则影响整个项目的成败。高效的电源设计直接有益于整个系统的散热,降低成品的成本和大小。低噪声电源解决方案可确保最终产品符合EMI标准,如IEC EN61000。在一些数据收发器和DAC/ADC应用中,其产品性能高度依赖于电源设计和EMI抗干扰水平。

原文发表在 Power Electronics Europe - September 2018.

2018.9
文章:一个充电 IC 的 N 种玩法

USB端口由于其普遍的兼容性和减少了电子垃圾的丢弃,被便携式设备广泛使用。此外,随着USB Type-C的普及,现在可以从标准的USB电源中汲取15W的功率,而不需要增加支持USB电源传输的成本。

MP2639A具有功能多样化、控制灵活性和高可靠性等优点,是各种应用的理想选择,如电子销售点(POS)机、蓝牙音箱、电子香烟、移动电源等。在本文中,我们将介绍使用MP2639A的各种应用。

原文发表在 Bodo's Power Systems (page 36).

2018.8
网络研讨会:揭秘汽车EMI

达到严格的汽车EMI/EMC标准,成为尖端资讯信息、ADAS和照明系统硬件工程师一大头痛之事。此次 揭秘 EMI 网络研讨会就这一热门话题展开讨论,充分解释什么是 EMI,其产生的原因,以及如何降低干扰。

详见研讨会QA部分问题及答案

2018.6
文章:驱动电磁线圈的最佳方法

电磁线圈作为相对简单的电气机械装置,常常用来将电能转换成线性运动/驱动。然而,驱动电磁线圈也会存在一些挑战。在“驱动电磁线圈最佳方法 一文中我们提出的方法不仅提高了产品性能,还解决了一些挑战难题。

原文发表在 Electronic Design

2018.5

文章:介绍 MagAlpha MAQ430 & MAQ470: 12-位、汽车级、磁角传感器

随着现代汽车开始集成越来越多的技术和系统来帮助驾驶,汽车角运动或旋转的测量也变得越来越重要。如今,许多汽车系统选项可以通过单个旋钮选择器来控制,且先前的手动功能被逐渐机动化,这便要求电机旋转、位置和速度控制。

本文探讨了如何使用 MPS 的 MagAlpha MAQ470 和 MAQ430 汽车级角传感器为您提供高度可靠和非接触方式的角度、旋转位置和速度测量。

原文发表在 CODICO Impulse

2018.5
 文章:课堂上学不到的知识点—关于同步整流器 – 学习实用的AC DC设计技术

近年来,为了进一步改善全球节能,全球监管机构提出了新的效率标准。随着美国能源部(DOE)出台的一系列新要求,制造商必须提高现有独立电源产品的效率以达到DOE VI级标准,才能在美国市场销售。此外,制造商还需要设计符合其它能源规格的产品,例如欧盟CoC V5 Tier2规格。

原文发表在 Bodo's Power Systems.

2018.5
文章:MPS 可扩展模块 — 让大电流设计更加简洁

如今,由于FPGAs和ASIC的快速普及,也给电源模块设计带来了一定的挑战 —— 应用需要更宽的无线网络带宽来驱动,而数据中心则需要更高的功率密度、更快的负载瞬态响应和更智能的功率管理功能。因此,理想的电源模块解决方案需变得更加紧凑、人性化可定制、易于使用,同时功率传输能力绝不可输于传统设计。

原文发表在 Power Electronics Europe.

2018.5
文章:奔驰 E 级 USB 充电模块拆解报告--MPQ448x

大家都用手机,但不一定知道目前国内车厂出现了一台神奇的设计,12个USB充电口,像装修房子一样。而其实汽车电源的设计具有特殊性,想要把单个USB的充电器做好,单就保护还有电压移植的工作就已经很不容易, 12个谈何简单。我们的最新文章将带您揭开这一神秘面纱。

原文发表在 WeChat (中国)。

2018.1
文章:采用两级电源架构方案提升48V 配电系统功率密度和数据中心能效

当前的数据中心,通常仍需要一个 12V 背板以及板上配电功能,并采用单相或多相同步 Buck 降压调节器,方可将电压降到 1V 左右。正常情况下,这些数据中心机架的额定功率最大为 20kW。而业内的需求是希望将每个机架的功率密度能提高到100kW,从而减少整体尺寸。其实,完全可以通过使用 48V 背板和配电来实现这一需求,然而这种方法却存在诸多挑战,因为它无法依靠传统同步 Buck 降压调节器将48V 电压驱动至电路板。那么,还有什么其他办法可以在不增加成本的前提下提高数据中心的功率密度呢?本文概述了一种两级架构解决方案——以一种灵活的、可调节的、高性价比方式,将 48V 电压驱动至负载点(POL,大约 1-5V),这对于下一代服务器功率传输将大有裨益。

原文发表在 Power Electronics News.

2017.10
文章:MPS Smart Ramp 技术 - 变压解决方案 - 降低可闻噪声

稳压器(VR)系统中的可闻噪声是一个长期存在的问题。在PC工业中,显著而重复的电压变化主要来自于CPU,而这些电压变化会通过VR产生噪音,因此这个问题变得更加突出。电压的变化以及陶瓷电容器和底板的物理特性,给PC制造商带来了可闻噪声问题,迄今为止没有更好的解决方案。MPS Smart-Ramp 技术将为您解决电压变化引起的可闻噪声问题。

原文发表在 AllAboutCircuits.

2017.5
文章:Total Integrated Power Solution for Smart Lighting

Smart lighting is considered to be the new frontier of the global lighting industry, as the trend of smart homes, Internet of Things (IoT), and a connected world are the main driving factors in global electronics growth. In terms of major applications of the smart lighting concept, the industry is currently more focused on light intensity dimming, lighting color temperature adjustment, ambient sensing, and monitoring. However, in the future, smart lighting applications can extend way beyond this range, the smart lighting devices can be used as a hub, integrated as key component of IoT systems and smart home/smart automation networks. This article will focus on the power solution for smart lighting- in particular smart light bulbs.

原文发表在 Power Electronics Europe.

2017.4
文章:Tackling Automotive Lighting's Common Challenges with New LED Driver Modules

LED lighting is one of the fastest growing segments in automotive electronics, but it is not without its own unique challenges. This article describes several major constraints facing today’s lighting designers and explores how these can be addressed by MPS’s new MPM6010-AEC1 automotive LED module.

原文发表在 Codico Impulse.

2017.3

分析和仿真PCB 交流电阻损耗,优化DrMOS核心电压