Total Integrated Power Solution for Smart Lighting
By Zhihong Yu, AC/DC Product Marketing Manager, Monolithic Power Systems
DOWNLOAD PDFSmart lighting is considered to be the new frontier of the global lighting industry, as the trend of smart homes, Internet of Things (IoT), and a connected world are the main driving factors in global electronics growth. In terms of major applications of the smart lighting concept, the industry is currently more focused on light intensity dimming, lighting color temperature adjustment, ambient sensing, and monitoring. However, in the future, smart lighting applications can extend way beyond this range, the smart lighting devices can be used as a hub, integrated as key component of IoT systems and smart home/smart automation networks (1).
This article will focus on the power solution for smart lighting- in particular smart light bulbs.
Government initiatives regarding the installation of the smart lighting system, the popularity and affordability of wireless control, and growing awareness regarding the benefits of smart lighting systems are other key factors boosting the demand for smart lighting solutions globally. According to a 2017 study from Research and Markets, the global smart lighting market is projected to witness a compound annual growth rate of 25.44% to reach a total market size of US$21.2 billion by 2022 from US$6.8 billion in 2017 (2) .
Referring to the teardown reports of some of commercially available smart light bulbs (such as Cree Connected Bulb (3) or Philips Hue (4)), the main structure of these bulbs are fairly similar (see Figure 1). A constant-current (CC) LED driver (such as the MPS MP4027) drives the main LEDs in addition to a constant-voltage (CV) buck driver (such as the MPS MP15x and MP17x) and provides either 5V or 3.3V to power the Zigbee/Wifi/Bluetooth/other transceiver IC and main microprocessor. The microprocessor in addition to the transceiver IC allows end users to control the lighting remotely using a mobile device. This control module sends a pulse-width modulation (PWM) or other digital signal (such as I 2C) to control the dimming of the LED driver.
Figure 1: Current Popular Smart Lighting Power Structure
While this topology seems ideal, this power stage faces two challenges: further minimizing the solution size and further decreasing standby power loss.
A19 and PAR bulb sizes follow industry standards and will not increase. Adding smart lighting functions to normal light bulbs means that the designer must squeeze more electronics into the same space, which is a big challenge, and the space limit may force designers to use fewer LEDs or use less LED power for easier thermal management. Sometimes, designers must adopt customized PCB shapes to fit all required electronics, which add to assembly cost.
Additionally, customers and legislation agencies are gradually noticing the importance of standby power consumption. Designers are expected to design smart lighting devices with super-low standby power to make the product attractive or sellable in certain regions with stringent energy consumption standards. For example, the European CoC Tier2 requires all external power supplies under the 49W power rating to have a standby loss of no more than 75mW. Smart lighting products are in the same way expected to meet certain energy specs in the near future (5). Currently, many smart light bulbs have high standby loss due to wireless circuitry power usage, which is inevitable, and therefore the standby loss can only be saved from the power stage.
To further shrink the size of smart lighting circuits and lower standby loss, a better integrated total power solution is presented in Figure 2. Here, the CV and CC circuits can be merged into a single-chip solution, shrinking the circuit BOM and standby loss.
Figure 2: Transition from Existing Power Stage to New Power Solution for Smart Light Bulbs
By adopting the solution shown in figure 2, circuit designers can eliminate one control IC, one external inductor, and other resistors and capacitors, cutting PCB space and BOM cost by at least 20 - 30% in the power section of a smart light bulb (see Figure 3).
Figure 3: BOM Comparisons between Existing Power Stage and New Power Solution
Furthermore, this solution can achieve less than 20mW of system standby power since the power section is highly integrated and more IC blocks can be left in the hibernating status at power off with an optimized, minimal operating frequency at no or light load.
The operation mode of the MP4057A is summarized in Figure 4. During start-up, VDD is supplied by the N_Forward winding. Then the IC determines whether it should run in CV mode (to power the MCU only while the LED remains off) or CC mode (to power both the MCU and LED) by monitoring the DIM pin, which is controlled by the MCU itself.
During CV mode (DIM pin is low), VCC acts as the supply to the IC. The ratio of N_flyback and Ns winding can be adjusted so the LED will not light up in CV mode. There is also a smart frequency modulation algorithm implemented to ensure low standby power and fast transient response to LED load changes, as well as ensuring there is no voltage drop at the MCU power, and no LED flickering during CV/CC transition.
Figure 4: Control Method Reference
If DIM senses the PWM signal from the MCU to control dimming, then the IC enters CC mode. The feedback voltage is modulated by reading DIM to modify the LED current based on the DIM duty cycle while keeping the CV output constant. As under CC mode, the MCU Vo pin must also be high enough, hence the IC is limited to a 5% minimal LED dimming depth to provide enough voltage to drive the MCU. The Vo power loop is decoupled from the main LED current loop by setting the ratio of current sense resistors (Rs1 and Rs2).
For LED current control, this solution implements a constant on-time (COT) control method, which also guarantees a high power factor. The on/off transition occurs during valley switching (by sensing through a zero-current detection (ZCD) pin) to eliminate turn-on loss and diode reverserecovery loss, which is also referred to as transition mode control. The IC also includes other features, such as minimum off time (to improve EMI), leading-edge blanking, over-voltage protection (OVP), over-current protection (OCP), over-temperature protection (OTP), and more.
Figure 5 shows LED load efficiency and power factor performance, and Figure 6 shows a very linear PWM dimming performance. Figure 7 shows an 8W reference design circuit board suitable for all kinds of PAR lamps. For ordering information, MP4057A offers 3.3V for MCU power, while MP4057B offers 5V.
Figure 5: LED Load Efficiency and Typical Power Factor
Figure 6: PWM Dimming Ratio
Figure 7: Evaluation Board EV4057A-K-00A:
(L x W x H) 66mm x 25mm x 15mm
230Vac/50Hz Input, Isolated Flyback Converter, VLED = 21V, ILED = 0.37A, Vo = 3.3V, Io = 50mA
To summarize, the IP-protected solution offers higher system density and lower cost compared to existing solutions. For a complete list of AC/DC and lighting controller offerings, please visit our LED Lighting & Illumination page or contact your local MPS sales office.
____________________________________________________________________________
- http://www.researchandmarkets.com/research/8bnwls/smart_lighting
- Lighting, LED and smart lighting market overview: https://energy.gov/sites/prod/files/2016/02/f29/smallwood_mktadoption_raleigh2016.pdf
- Cree Connected LED Bulb Teardown: https://www.youtube.com/watch?v=q-hLMCeCnj0
- Philips HUE (2016) LED Bulb Teardown: https://www.youtube.com/watch?v=4L1ZqvQ2qVU
- New group pushes standards for IoT luminaires 2017/05: http://www.ledsmagazine.com/articles/2017/05/new-group-pushes-standards-for-iot-luminaires.html
Did you find this interesting? Get valuable resources straight to your inbox - sent out once per month!
Technical Forum
Latest activity 6 days ago
2 Comments
Latest activity a week ago
2 Comments
Latest activity a month ago
2 Comments
Log in to your account
Create New Account