MPS > PressReleaseList > MPS Launches Industry's First Programmable Power Product Family  

Press Releases

MPS Launches Industry's First Programmable Power Product Family 

Content

San Jose, CA, Jan. 27, 2014 Monolithic Power Systems (MPS) (Nasdaq: MPWR), a leading fabless manufacturer of high-performance analog and mixed-signal semiconductors, announced today the release of the MP2953,  the  industry's first fully-programmable controller specifically designed for Information/Communications and cloud based systems including server core, memory, storage and any DC/DC application where efficiency maximization is critical.

MP2953, a fully-programmable 6-Phase Controller with telemetry and Auto-Loop Compensation, is the first product introduced in the programmable power family, targeting ultra-compact, high density VR/VRM systems. The
proprietary process technology utilized in this product enables MPS to leapfrog its competition in terms of power density, ease-of-use and reduction in size and bill of materials. Coupled with MPS’s family of Intelli-Phase™ DriverMOS IC’s, the MP2953 also delivers the best-in-class performance in efficiency and transient response. The Current Sense technique built into MPS Intelli-Phase IC’s allows the MP2953 to monitor and report output current at an extremely accurate level eliminating the need to overdesign your system while delivering the most optimized power and efficiency.

Further, the programmability by software implementation using MPS proprietary graphical user interface (GUI) eliminates the need for traditional "trial and error" design processes in the lab. Therefore, virtually all parameters are very easy to program or monitor by using the IC's telemetry feature and program through the MPS GUI interface. MPS GUI used to program the device is the most user-friendly interface on the market today and offers an intuitive control features that allows the power engineer to complete their design and evaluation in short order. The MP2953’s digital power management and control features provide real-time intelligence which allows the system designer to build a system that adapts to their conditions while optimizing efficiency. Finally, MPS’s proprietary auto-tune technology allows for changes in the load and temperature enabling power savings under even extreme light load conditions.

I'm very pleased with the positive feedback from our customers and am particularly proud of our software and silicon designers who developed this innovative solution.  Our programmable power product family set us apart from the competition. We feel that we have succeeded in introducing the easiest to use and the best performing digital solutions out there today,” said Michael Hsing, CEO of Monolithic Power Systems (MPS).

About Monolithic Power Systems

Monolithic Power Systems (MPS) is a fabless semiconductor company specializing in high-performance analog ICs. Founded in 1997, MPS's core technology is its innovative and proprietary manufacturing process combined with superior analog circuit design capabilities across system-level and end customer applications. These combined advantages enable MPS to deliver highly integrated monolithic products that offer energy efficient and cost-effective solutions. MPS product families include DC/DC converters, LED drivers and controllers, Class-D audio amplifiers, battery chargers and protections, USB and current-limit switches and AC/DC offline products. MPS has over 1,000 employees worldwide, located in the United States, China, Taiwan, Korea, Japan, Singapore and across Europe.

###

Monolithic Power Systems, MPS, and the MPS logo are registered trademarks of Monolithic Power Systems, Inc. in the U.S. and trademarked in certain other countries.

Contact:

Jae Park

Marketing Communications

Monolithic Power Systems, Inc.

408-826-0798
jae.park@monolithicpower.com

Date

1/27/2014 
©2010 Monolithic Power Systems, Inc. All Rights Reserved